STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F xxx Strange USB File Write Error - HS Mode Only

Posted on February 10, 2014 at 17:31Hi,I am getting a strange file write error when using HS USB lib and FATfs. this error does not occur in FS mode.When I write 2 bytes to a file and then 1024 bytes, some (2)  of the 1024 bytes are repeated at 0x20...

0690X000006052HQAQ.png
louis by Associate II
  • 2158 Views
  • 5 replies
  • 0 kudos

MCBSTM32F200 MicroController NRST signal

Posted on February 11, 2014 at 01:33I have started using the MCBSTM32F200 eval board but I cant figure out how to control the NSRT signal. It says J1 next to it on the schematic but I don't know that means. #nsrt #stm32

r_zijoo by Associate II
  • 1928 Views
  • 4 replies
  • 0 kudos

Can't transmit over SPI with DMA

Posted on March 21, 2013 at 19:21 I am using an STM32F4, and I'm having difficulty getting SPI to transmit using DMA. If I manually write to the SPI data register, I see the appropriate activity on the logic analyzer, but if I use DMA to initiat...

order by Associate
  • 4682 Views
  • 16 replies
  • 0 kudos

STM32F405 - measure two frequencies >= 10MHz

Posted on January 27, 2014 at 11:46Hey at all, First of all I want to say that my english isn't the best. I have got a new project to do it on a STM32F405 controller. I must measure two frequencies: 1. f1 = 13 to 16MHz 2. f2 = 10 to 13MHz my plan to...

EVALST7590T-2

Posted on February 10, 2014 at 16:27hi, i have 3 EVALST7590T-2, I would like to know if the boards are set as the default service node or as a base node and how to do and where to get the files to set them as a base node or service node. Thank you ...

STM32F Standby PowerManagement

Posted on February 09, 2014 at 16:40Hi, in my project a 2.8V voltage regulator is connected to the VDD pins of the STM32Fxx device. VBat is directly connected to a 3V battery. After reset the mcu processes some tasks and after that the controller f...

Trouble reading SD Card SCR Register with SDIO Peripheral

Posted on February 01, 2013 at 16:03I'm trying to read the SD CARD Configuration Register (SCR) on an SD memory card using the SDIO peripheral and I'm not sure if I'm approaching this in the right way, so I'm hoping someone here may have some experi...

dohzer by Associate II
  • 2227 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.