STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

GPIOx_OSPEEDR and GPIO Compensation Cells

Posted on February 19, 2014 at 23:36Hi AllI've been working with STM32F405/07 (STM32FDiscovery & my own designs) for a while now... though I'm certainly no expert:) This is a request for any discussion or useful information generally related to high...

rgodshall by Associate II
  • 3583 Views
  • 4 replies
  • 0 kudos

Write to textfile

Posted on February 19, 2014 at 09:35Hi I'm trying to write some values to a textfile but without success. I work with the IAR Workbench. Bellow the code which I found also in the Arm User Guide:#include <stdio.h> FILE *f; f = fopen (''Test.txt'',''r...

csutter by Associate
  • 1816 Views
  • 3 replies
  • 0 kudos

Injected ADC Conversion Time off by 1.2usec

Posted on February 20, 2014 at 16:37I am using TIM1 (PWM Mode) to trigger injected adc conversions in dual mode.  The ADC clock is set to 72 Mhz (PLL Clock).   The ADC sampling is set to 19.5 cycles --> a total conversion time of 19.5 + 12.5 = 32 cy...

richard23 by Associate II
  • 2660 Views
  • 5 replies
  • 0 kudos

STM32F103ZE TIM1 InputCapture

Posted on February 19, 2014 at 17:16HI, I'm trying to configure TIMER1 CHANNEL2 for InputCapture to measure a pulse from some external hardware. My init code looks like this:  ////////////////////////////////////////////////   // Enable Timer1 clock...

I2C with MCCOG21605B6W 16 Character LCD

Posted on January 08, 2014 at 14:24 Hello all, I am using the STM32VLDISCOVERY board which has a STM32F10x controller. I am trying to communcate with the LCD, but I am facing problems. Here is my code: // Master mode I2C1->CR2 ...

0690X00000603GzQAI.jpg
tan by Associate II
  • 2366 Views
  • 6 replies
  • 0 kudos

SPI communication between 2 STM32

Posted on February 19, 2014 at 10:34      Hello everyone,   I would like to use SPI protocol in order to communicate between two µC STM32f429.  One will be a master, and the other one will be slave.   I would like to perform very easy operation to b...

INTERRUPTS on STM32 F4 discovery

Posted on February 18, 2014 at 04:34Hello Everyone, I need help to implement 2 different interrupts in order to : detect the falling edge of the signal (1)detect the rising edge of the clock (R3) 120kHzAny help will be very appreciated. Thanks ...

0690X00000603HEQAY.jpg

How to use STM32L152 Internal Ref for ADC?

Posted on February 19, 2014 at 15:28Hello,I'm using  STM32L152 64pin MCU and don't know how to enable internal 1,2V Ref voltage for the ADC1.The ADC works well but is seems to use Vref+/- pins (I have ca 2,8V at these) by default.Btw. I'm on Discove...

Tom by Associate II
  • 1139 Views
  • 6 replies
  • 0 kudos

Dual core stm32f4

Posted on February 20, 2014 at 08:45For many control applications that we have a fast control loop that can not be interrupted and also have communications on CAN,USB,RS485,Ethernet,...it is better to have a dual core stm32 that one core must be Cor...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.