STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Current Consumption

Posted on April 02, 2014 at 10:49Hi all, I'm using the F3 Discovery. I want to use an external board by powering it using the external application power supply 5V of my Discovery.  I measured my the current consumption of my discovery alone and it's...

hilwan by Associate II
  • 3456 Views
  • 8 replies
  • 0 kudos

Parse HTTP header

Posted on April 02, 2014 at 21:06 Hi, I use LwIP stack with FreeRTOS and STM32F4 Discovery. I use it like web server. And I want parse POST parameters. And parse header for read Cookies. I wrote lot of functions. Some functions was good in on...

zavodny by Associate II
  • 1498 Views
  • 2 replies
  • 0 kudos

Resetting IT Pending bit for CAN interrupt

Posted on April 03, 2014 at 08:27 Hello, i am working with a STM32f103 with the integrated CAN controller and i use the std. periph library. In the function CAN_ClearITPendingBit(CAN1, CAN_IT_BOF); the entire CAN_MSR reg...

STM32F4DISCOVERY VBAT pin

Posted on March 31, 2014 at 17:10Hi all, I want to use RTC from STM32F4DISCOVERY and have a doubt about VBAT pin that is connected to VDD through R26 0Ohm, this are saying that I need to take off R26 to plug a vbat battery, but if I take off the R26...

ppsilv by Associate II
  • 3044 Views
  • 6 replies
  • 0 kudos

stm32f4xx FLASH_ProgramWord error, FLASH_ERROR_PROGRAM

Posted on April 02, 2014 at 16:13 Dear, i am getting this error, this is my flash write routine: #include <stm32f4xx_flash.h> #include ''flash.h'' uint8_t flash_status; volatile uint32_t* flash_location_sect3 = (volatile uint...

Angelo1 by Associate II
  • 2638 Views
  • 7 replies
  • 0 kudos

stm32f405 help for timer seconds counter

Posted on April 01, 2014 at 18:47Dear, i need to implement a timer, with seconds step, just as a watch. I have now the follwing clock (internal) set static void SetSysClock(void) {         /* PLL (clocked by HSI) used as System clock source */      ...

Angelo1 by Associate II
  • 1357 Views
  • 3 replies
  • 0 kudos

I2C problems

Posted on March 26, 2014 at 16:10HiI'm trying to write and read some data into a EEPROM (AT24MAC402) with my STM32F417 in I2C but the program loops in the START and don't write or read in the EEPROM. There is a status in ''stm32f4xx_i2c.c'' that sta...

tiche79 by Associate II
  • 6565 Views
  • 10 replies
  • 0 kudos

Hard Fault Writing Flash

Posted on March 28, 2014 at 16:11Hi, i'm trying to create a bootloader into the component STM32f106RDT with 384KO of Flash. I have mapped the memory like this: 0x08000000 - 0x0802FFFF for main software (first binary) 0x08030000 - 0x08030FFF for boot...

tommelou by Associate II
  • 3576 Views
  • 5 replies
  • 0 kudos

STM32L1 OPAMP1 Gain Error

Posted on April 02, 2014 at 15:28 Hello All, I connected DAC1 output (S6 closed, S5 opened) to the internal OPAMP1 AIN+ which is in noninvering configuration by two external resistors (Rf=150k, Rg (to ground)=50k) which should yeld G=x4 ...

Tom by Associate II
  • 1178 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.