STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ST MDK5 CMSIS device driver packs examples

Posted on May 09, 2014 at 15:48Hi, Has anyone started using V1.0.7 Keil.STM32F4xx_DFP.1.0.7.pack? We are considering  to use it as a part of medical product development. I also do not see any example codes as a part of this pack (particularly requir...

vasanth by Associate
  • 704 Views
  • 0 replies
  • 0 kudos

STM32F0 ADC Temperature Drift?

Posted on May 08, 2014 at 17:48Simple question - should be answered in datasheet, errata sheet, or ref manual but I cannot seem to find it. I am wondering how much ADC readings drift relative to the reference voltage with temperature. If I have a co...

Tutorials, etc.

Posted on May 06, 2014 at 07:17Is there a tutorial or lecture series for beginners working with a STM32F3 demo board? I have programmed simple project boards like Arduino, but not anything like the STM32 boards. I have tried to work backwards from t...

jprevard by Associate II
  • 5153 Views
  • 11 replies
  • 0 kudos

stm32f405, lock question

Posted on May 06, 2014 at 00:33Dear, i have the following issue: i have seen that i cannot process too many instructions from inside interrupt. I guess there is a limit. (still didn't looked the datasheet), So i decided to do just some few operatio...

Angelo1 by Associate II
  • 3075 Views
  • 7 replies
  • 0 kudos

STM32F205ZGT6 - PC13 as output doesn't work

Posted on May 08, 2014 at 20:36 Hello, I'm trying to use the PC13 as an output but I can't get any signal change from it. I'm already setting the pins PC14 and PC15 as inputs following the datasheet orientations. I used one of the ...

gui by Associate
  • 1037 Views
  • 1 replies
  • 0 kudos

How to access *any* memory address without a bus fault?

Posted on May 08, 2014 at 11:57How could I write some code that would access a memory address and wouldn't generate a bus fault if it was incorrect? Or failing that, is there a way to safely check if an address is valid, or maybe even a way to have ...

gw by Associate II
  • 6387 Views
  • 20 replies
  • 0 kudos

Problem with file creating on SD card with FatFs lib

Posted on April 16, 2014 at 12:36 Hello, I use a STM32F427 running with FreeRTOS. I try to create a file on my SD card, through SDIO, thestm32f4_discovery_sdio_sd.c (DMA mode). I also use the librairyFatFs R0.09, ported by Clive I ...

Bit width of the SDRAM on STM32F439 MCU

Posted on May 08, 2014 at 14:37Hello! Is there any goal in use a 32 bit SDRAM memory VS the 16 bit SDRAM memory on STM32F439 device? I want to transfer a 30 fps video from DCMI to 4.3 LCD. Wich SDRAM will be faster? 16 or 32 bit?

ivandevel by Associate II
  • 1202 Views
  • 1 replies
  • 0 kudos

stm32f303vct debugger fault

Posted on May 07, 2014 at 16:56stm32f303 debugger is not working .controllerdoesnt power up with usb connection with laptop but when i supply external supply of 3v it powers up but debugger still not working .what could be the fault ? #stm32f303v...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.