STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I2C Reading state machine

Posted on April 11, 2013 at 23:50Hi,I am working on STM10C eval board. I am trying to read X and Y datas from the touchscreen using a state machine inside the I2C_IRQ_Handler. The start byte is generated inside the EXTI interrupt once a touch is det...

GSM Modem Interference

Posted on June 23, 2014 at 10:13A GSM modem is in proximity to the uC. When the current bursts of the modem occur I get false logical 1 on my port pins. They are configured as analog inputs. I am using the STM32L100-DISCO board. I was wondering if t...

abuelmagd by Associate II
  • 4030 Views
  • 5 replies
  • 0 kudos

Accurate RTC using HSI

Posted on June 23, 2014 at 21:14I'm using the SMT32F030 with 48MHz internal clock. I've configured the RTC and noticed it is about 8% fast. Is there a way to make this more accurate through calibration of some sort? Will that have to be done from pa...

daniel2 by Associate II
  • 820 Views
  • 1 replies
  • 0 kudos

vaiable to a personal computer

Posted on June 23, 2014 at 12:08I use stm32f4 discovery.how can I send a value of a variable to a personal computer?exist an example?

cchechio by Associate II
  • 1045 Views
  • 1 replies
  • 0 kudos

STM32Cube stack alignment problem?

Posted on June 23, 2014 at 14:34 STM32Cube ld scripts set _estack to the last location of RAM like this: /* Highest address of the user mode stack */ _estack = 0x20017FFF; /* end of RAM */ I had several problems with code that u...

whg03 by Associate II
  • 2413 Views
  • 4 replies
  • 0 kudos

stm32f429-disco and beginners question

Posted on June 20, 2014 at 15:26 Hi, as a beginner I am starting freshly with stm32 programming on a stm32f429-disco board using eclipse with the gnu-arm-plugin and the gnu-arm-eabi toolchain in linux (toolchain is working - the simple LED-b...

STM32F4Cube HAL_SPI_TransmitReceive_IT()

Posted on June 19, 2014 at 21:42Hello, I am interfacing an STM32F407 (on DISCOVERY eval) to several devices using SPI bus.  One of the devices clocks 4 bytes of data out simultaneously as 4 bytes of config data is clocked in (LTC2446 ADC).  I am att...

DMA reads from USART1 without RXNE set

Posted on May 06, 2014 at 12:11Hi community, I use the USART1 in STM32F100C4 to receive serial data in DMA mode. Because the data comes in packets with less than 16 bytes I start the DMA mode every time, when new data is expected. This works most of...

h2 by Associate II
  • 6424 Views
  • 16 replies
  • 0 kudos

High speed UART with DMA

Posted on June 20, 2014 at 12:18Hi, I'm working on a STM32F4 mcu and I'd like to use an UART with a baud rate of 1843200bps with a DMA that works for every byte received on this UART. Using CubeMX I have created an example code with a UART 1843200b...

DUrbano by Associate III
  • 5326 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.