STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ETH PPS signal generation in PF10

Posted on October 09, 2014 at 13:31Hello everybody! I am working with STM32F437ZGT6 device and using PTP processing. This appears to run OK. Now I must generate a pulse-per-second signal (PPS) with the Ethernet module. The main problem is that pins ...

0690X00000605AoQAI.png
Jose_A by Associate II
  • 2946 Views
  • 2 replies
  • 0 kudos

STM32L151 Stop mode problem

Posted on October 14, 2014 at 11:13 Hi all! I faced problem with STM32L151 and i hope to find some useful considerations. The problem is following. I use stop mode with RTC. RTC is configured with periodic wake-up timer. I also use exte...

STM32F4: Bootloader: CAN bus

Posted on July 14, 2014 at 14:51I am trying to load firmware over the CAN2 bus using the STM32F4's internal bootloader from a Linux system following the application note AN3154. In general this is working but I have an issue when writing the data us...

Timer interrupt incorrect result

Posted on October 13, 2014 at 18:27Hi everyone. I need some explain why this code generating not 1KHz TIM2 interrupt. I have no idea why generating 2KHz in APB1 clock(30MHz) & PPRE1(0b101) & CKD(0b00).#include ''stm32f2xx.h'' void TIM2_IRQHandler()...

Obtaining image using STM3220G-EVAL

Posted on October 13, 2014 at 16:30Hello,I'm using the STM3220G Eval board and the camera (OV2640) present on the eval board to obtain a RGB image on MATLAB.The image mode is set to QVGA. As per standard, the image size of QVGA is 320X240 pixels, bu...

0690X00000605YlQAI.png 0690X00000605YqQAI.png

One thread use up all the computer time,which use ADC.

Posted on October 07, 2014 at 16:46 I am adding a thread to STM32F429iDisco demo. This thread use ADC, it use all all the computer time, other thread do not response at all. I try to add code:  vTaskDelay(1000); or  GUI_X_Delay(1000) It still doesn...

Linda by Associate II
  • 2120 Views
  • 7 replies
  • 0 kudos

STM32F103 CAN Transceiver

Posted on October 10, 2014 at 16:15Hello everybody,I am searching for a CAN transceiver for STM32F103 based board I am developing.I was interested in the AMIS-30633 transceiver, it is automotive certified and it is ISO 11898 compliant. The STM32 CAN...

emilio by Associate II
  • 1849 Views
  • 3 replies
  • 0 kudos

STM32L100RB Faulty USB SIE???

Posted on October 04, 2014 at 09:18I've been spending quite some time trying to get the VCP from STSW-STM32121 to work on my STM32L100RB project to no avail and this is what I have found. DP is being pulled up by the 1.5kohm resistor but never does ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.