STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F3 DMA and concurrent memory access

Posted on October 22, 2014 at 11:00Hello, I'm new in STM32 World. I have a question:I enable ADCs in my STM32F3 with dma access and microcontroller works very well, but, in F3 is not possible double buffering or pinpong method with dma, correct?So, ...

lrosadev by Associate II
  • 1134 Views
  • 1 replies
  • 0 kudos

BSDL files for STM32F373

Posted on October 22, 2014 at 11:51I have tried to locate a BSDL file for STM32F373VCT6 ? anywhere to be found?//Pierre

ekapiwi by Associate
  • 1016 Views
  • 1 replies
  • 0 kudos

HAL_SPI_TransmitReceive_IT() never completes

Posted on October 20, 2014 at 13:10I am having an issue with the STM32Cube HAL function, HAL_SPI_TransmitReceive_IT(). I am using the STM32CubeF2 library with STM32CubeMX tool to generage most of the initialisation code.I have an STM3220G evalutatio...

andrew by Associate II
  • 3491 Views
  • 5 replies
  • 0 kudos

RDP and PCROP spurious activation

Posted on October 22, 2014 at 09:52 Hi, I have a flash init routine that I call after enabling the main PLL in my boot loader and my main application. The routine will check in the bootloader if the OPTCR or OPTCR1 values have been changed fo...

mfm by Associate II
  • 2465 Views
  • 4 replies
  • 0 kudos

Loop problem on an STM32F4 Discovery

Posted on October 22, 2014 at 11:17Hi guys, I'm Aurelio, I'm 22 and I'm from Italy :)Yesterday I bought an STM32F407VGT6 Discovery board, but I have a strange problem. I wrote this simple code to light the LEDs on the board when the user button is p...

aurelio by Associate
  • 698 Views
  • 0 replies
  • 0 kudos

STM32L152VC: LCD segments not all 5V tolerant

Posted on October 21, 2014 at 19:36The STM32L152VC includes an internal voltage regulator with contrast control from 2.60 to 3.51V. Those voltages then get used to drive the individual segments. In my case, I'm running the processor at 2.6V (VD). Wh...

sheldon by Associate II
  • 1120 Views
  • 1 replies
  • 0 kudos

Hard fault error and static variable

Posted on October 15, 2014 at 10:14Hello all, Following some hardfault error with my code running into a STM32F415, I found a solution that leave me puzzled. In my main, I declare a array of 600 uint8_t called data;uint8_t data[600]; I call a funct...

ARM GCC + STM32 don't like each other

Posted on October 16, 2014 at 16:29Hello matesI'm looking to use the SMT32F303VC (STM32F Discovery Board) for my first product. I'm developing on mac osx, build my toolchain based on ARM GNU GCC (GCC ARME NONE EABI 4.8) + Eclipse + Zylin Plugin + Op...

STM32F4 Discovery slow speed

Posted on October 21, 2014 at 00:00 Hi all, I am working with the STM32F4 Discovery board and I changed the Standard Periph Library from 1.0 to 1.4 With the 1.4 version the boards run slow with this code: #include ''stm32f4xx_c...

danelifab by Associate II
  • 1919 Views
  • 4 replies
  • 0 kudos

Sending ten bits to SPI slave

Posted on October 18, 2014 at 20:19Hi, I want to send ten bits from my STM32F4 Discovery to a SPI slave. The SPI Init struct only allows 8- or 16 bit (SPI_DataSize_8b, SPI_DataSize_16b) Whats the best way to send the required ten bits to the SPI sla...

paul2 by Senior
  • 1282 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.