STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to send DATA from Slave to Master over SPI

Posted on November 17, 2014 at 16:12Hey guys I'm think to send data from Slave to Master over SPI but there is a problem. when I send the dummy data on SPI lines for create clock on SCK line for Slave, How can I send the data from slave to Maser whe...

Cubemx 4.4.0 rtc bug

Posted on October 17, 2014 at 21:30 Hello everybody! I found a bug with the new cubemx and rtc clock code generation. So I set te RTC paramters at cubemx, the first what I see that the sync predivider limited to max 255, but this is ...

totti001 by Associate II
  • 2473 Views
  • 4 replies
  • 0 kudos

STM32F4 Discovery Board and CooCox

Posted on November 17, 2014 at 03:38I have started to use CoIDE to build codes to STN32F4 Discovery board. Any advice for using ''only'' ST supplied peripheral drivers and libraries? I do not want to use CoIDE wizard to deliver required/ selected dr...

adnan by Associate
  • 1059 Views
  • 1 replies
  • 0 kudos

[Solved] DCMI on the 32F429IDISCOVERY

Posted on June 10, 2014 at 20:29 Hello, Relevant information: The camera is the OV76I am supplying power through the USB port of my laptop.Signals look fairly well with a scope.Feeding the camera with the HSE divided by two (MCO2)...

DMA 16 ADC channels

Posted on November 13, 2014 at 11:31Hi,I need examples or informations about DMA and ADC 16 channels. I saw examples where DMA manage 4 ADC channels.   Thanks

mosine by Associate II
  • 1663 Views
  • 3 replies
  • 0 kudos

Program execution stops during flash page erase

Posted on November 17, 2014 at 10:21Hi,There is an Audio-Codec connected by I2S to the STM32F407/401 with 48kHz. Every sample needs to be calculated as soon as it arrives to keep the latency between Analog In and Out as short as possible, which mean...

koster by Associate III
  • 1467 Views
  • 2 replies
  • 0 kudos

Hard fault with stm32 std peripheral library

Posted on November 13, 2014 at 12:23Hi, This is a pretty noob question but I'm going to ask it anyway, because it seems like I'm missing something. I've just set up new STM32F1xx and STM32L1xx projects based on the GNU ARM plugin for eclipse.  I'm w...

Two questions about the A/D

Posted on November 13, 2013 at 17:31 Hi, I am successfully running most of my software, and I am now debugging the A/D. I first used the examples verbatim, to understand what I am setting up. I gave now modified the code, and have two questions: Th...

gullik by Associate II
  • 2368 Views
  • 5 replies
  • 0 kudos

STM32F429 LCD and Images

Posted on November 14, 2014 at 03:46Hello everyoneCan someone explain to me in detail how to display an image on the touch screen? I have been looking for some kind of tutorial but I can't find any. I've been looking at the LCD_WriteBMP command, but...

stone by Associate II
  • 3037 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.