STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F429I-Discovery interfacing External LCD

Posted on January 14, 2015 at 19:12Hi guys,I'm currently trying to interface http://www.wvshare.com/product/4.3inch-480x272-Touch-LCD-B.htm with the STM32F429I-Discovery board, but I don't know where to start. After lines connection (for the moment ...

angeletti by Associate II
  • 1625 Views
  • 3 replies
  • 0 kudos

STM32F407 captured value two times bigger than expected

Posted on January 14, 2015 at 20:51 Hi, I have the MCU run SysClk at 168MHz, and I setup the timer to capture mode, but the returned value is two times bigger than expected. I checked the waveform of the toggled LED, it is correct, just the Time...

gavinli by Associate II
  • 1664 Views
  • 4 replies
  • 0 kudos

STM32F030 SPI Open Drain Support

Posted on January 15, 2015 at 22:22Hi,I have a question regarding open drain configuration for SPI communication in the STM32F030x Family of MCUs. I have successfully configured the SPI interface with open drain outputs and external pull ups (for co...

camilo by Associate
  • 1122 Views
  • 0 replies
  • 1 kudos

CUBE HAL C++ Support

Posted on August 21, 2014 at 20:20Hi,     I've been trying to use the new F4 HAL libraries for a project on the F429 Discovery board. I realise that this will involve a lot of C to C++ integration.My first issue is with the two enum typedefs in   @f...

shorai by Associate III
  • 1502 Views
  • 7 replies
  • 0 kudos

JTAG (I-Jet) with STM324x9I-EVAL

Posted on January 15, 2015 at 18:45Should this work? I have the I-Jet plugged into CN16 and am using it with IAR EWARM and running ''emuDiag 3.57.'' The STM324x9I-EVAL is powered via USB and I have modified project options to use this debugger.The t...

hbarta2 by Associate III
  • 929 Views
  • 0 replies
  • 1 kudos

STM32F405 - Change GPIO Direction Dynamically.

Posted on January 15, 2015 at 14:38 Hi, Consider me a newbie in ARM. For last few days I am trying to control a set of GPIO pins dynamically. What I want to do is, to change the direction (Input to output or output to input),of the GPIO dynam...

Is this UART really busy?

Posted on January 12, 2015 at 14:00I'm baffled by a bit of code that results in a lockup in my application (On n STM32F429I-DISCO) related to a UART receive ISR. The code receives characters one at a time as it needs to handle variable length messag...

hbarta2 by Associate III
  • 4748 Views
  • 3 replies
  • 0 kudos

STM32F429 LTDC driving SSD1289

Posted on February 21, 2014 at 02:40Hi all. I'd like to incorporate this LCD into my project: http://www.mcu-turkey.com/wp-content/uploads/2013/12/3.2pi-ssd1289.pdf but I'm not sure it's possible to drive it with the LTDC. The display doesn't have V...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.