STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F0 SPI CRCERR bit problem (with DMA)

Posted on January 30, 2015 at 04:06I seem to have a problem with the CRCERR bit in the SPI SR for a STM32F031. The CRC generator is turned on, and the RXCRCR gives the correct CRC for the message received. A string of bytes is sent (hex 81 02 00 00 ...

gahelton1 by Associate III
  • 2878 Views
  • 4 replies
  • 0 kudos

Using SPI4 in STM32F429 - what are the changes needed

Posted on February 08, 2015 at 15:05I want to use STM429 MCU's SPI4 .But when I checked stm32f4xx_rcc.h  it only provides upto 3 spi's gates.How can I add support for SPI4 ?What are the changes in the which files required inorder to achieve SPI4 wor...

Using SPI4 in STM32F429 - what are the changes needed

Posted on February 08, 2015 at 15:08I want to use STM429 MCU's SPI4 .But when I checked stm32f4xx_rcc.h  it only provides upto 3 spi's gates.How can I add support for SPI4 ?What are the changes in the which files required inorder to achieve SPI4 wor...

STM32F429i-Disco can not read file

Posted on February 07, 2015 at 03:32My  MCU of STM32F429i-Disco can not read the U drive that connect to CN6 , the light of U drive is on and flashing when Demo of STM32F429i-Disco try to read it. the MCU just can not detect these files, and shows '...

Linda by Associate II
  • 745 Views
  • 2 replies
  • 0 kudos

conversion of c to assembly

Posted on February 04, 2015 at 11:10Dear sir/mamAs i am working on data acquisition project , i am facing the timing problem and i am not able to access complete data from the simulator for the transmission speed of 10 KHz  and above , data is missi...

Keil - Failed to reset CPU -

Posted on February 07, 2015 at 11:43Hi,I have made my own pcb design using STM32F407VGT6 in LQFP100 package.I used the stm32f4 launch board schematic.I pulled down the boot0  and boot1 pins using voltage divider (10k//510).I connected 15  100nf caps...

clock set problem

Posted on February 06, 2015 at 17:47 hi all mcu stm32f103 VBAT pin I have connected the to battery mcu or external I have connected the 3.2 volts I have set rtc_setcount hour =23:59:59 hour = 0 now works no pr...

kemal by Associate II
  • 886 Views
  • 1 replies
  • 0 kudos

Uart in STM32F4

Posted on January 31, 2015 at 16:03I create a program for uart interrupt receiving by cubeMX in ARM-MDK. I want interrupt receivng from PC(when for example 0xFF received from pc by hyperterminal or docklight). I write bellow program. main() {    whi...

mikropart by Associate II
  • 4038 Views
  • 8 replies
  • 0 kudos

redirection

Posted on February 06, 2015 at 16:31Hi All, I'm developing an application with STM32F407, keil RTC rtos and keil libraries. I've implemented the redirection of the printf message as suggested in many examples. It works fine, and I see the applicatio...

davide2 by Associate
  • 635 Views
  • 1 replies
  • 0 kudos

Emwin button event

Posted on February 06, 2015 at 17:37Hey,In my project, I add some buttons on the dialog, but I have an issue on the button event. the click event WM_NOTIFICATION_CLICKED works well but th release WM_NOTIFICATION_RELEASED is never triggered, I have t...

kqian by Associate II
  • 733 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.