STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Struggling with HC05 Module for AT Command

Posted on February 13, 2015 at 16:57I'm getting some hard time trying to make my HC05 to execute an AT command from my stm32f4 , first it seemed that the problem was that the module was not in AT mode, now that i got it to enter AT mode it still is ...

monta by Associate II
  • 3021 Views
  • 7 replies
  • 0 kudos

RTC doesn't tick with HSE/128

Posted on December 22, 2012 at 17:11 I meet troubles with RTC on STM32F103RBT6. And it seems RTC in STM32 is very big problem. Many people have problem with RTC.STM32 has many restrictions for LSE crystal. Noname crystal from China which work...

urasinov by Associate II
  • 3680 Views
  • 8 replies
  • 0 kudos

STM32F1 bootloader issue

Posted on February 13, 2015 at 14:23Hello,in last batch from our supplier we have a problem with entering internal bootloader via USART1.Something probably changed in the processors, because previously, there was absolutely no problem. Now we have l...

zexx86 by Associate II
  • 1605 Views
  • 4 replies
  • 0 kudos

STM32CubeMX support for STM32W108HB

Posted on February 13, 2015 at 06:58I tried to configure STM32CubeMX for STM32W108HB but didn't see any STM32W options. Is there any way to configure STM32CubeMX for a STM32W?

connect AD converter 7903 with SPI from STM32F4

Posted on November 02, 2014 at 22:55Hello, I want to connect an AD converter AD7903 with the STM32F429 http://www.analog.com/static/imported-files/data_sheets/AD7903.pdf The AD7903 can be driven in a simultaneous sampling mode. It is show in the dat...

der-kyle by Associate II
  • 5008 Views
  • 8 replies
  • 0 kudos

STM32F103: noise on GPIO input signal causes weird behaviour

Posted on February 11, 2015 at 22:56Hi everybody,I am struggling against a weird behaviour on a input GPIO.The GPIO input circuit is a simple pull-up; due to other components connected to my board, there is sometime some noise injected into the GPIO...

amarchi by Associate II
  • 4306 Views
  • 4 replies
  • 0 kudos

stm32f4 + ov7670 + dmlcd-35rt double upscaled image

Posted on February 13, 2015 at 03:16i am working on a project with stm32f4 , ov7670  and dm-lcd35rt image output from my camera is doubled and also its colour is greenish  following is my register setting // Clock Settings // xclk 24M pclk 12M    {...

scholar by Associate II
  • 1064 Views
  • 0 replies
  • 0 kudos

APB Timers can exceed the APB domain max clock ?

Posted on February 12, 2015 at 16:57I have STM32F429I chip , I want to used timers , at the same time im running the APB1 at its max speed of 45 MHz . Now the clock provided to the APB1 timers will be double the clock of the APB1 domain by hardware ...

READ PROTECTION can't be removed

Posted on February 11, 2015 at 15:44We've got a new board and we can't flash them. I am sending an output from STVP > Programming  OPTION BYTE area... Removing *READ PROTECTION* option, this will ERASE all the device flash memory! < OPTION BYTE prog...

stst9184 by Associate II
  • 7438 Views
  • 13 replies
  • 0 kudos

6XUSART or UART mcu

Posted on February 11, 2015 at 13:03Hi all,I need a mcu with 6xUSART or UART.I couldn't find like it.Parametric search http://tureng.com/search/misguides me.Different data between parametric search and datasheet.Can you suggest to me a mcu like it.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.