STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Driver & USB version

Posted on March 26, 2015 at 17:10To add on the version for driver and USB device.STM32L0xx HAL Driver: V1.1.0STM32 USB Device Library: V2.2.0Kindly help if you know what could be wrong on the data receiving part. Thanks a lot.

hokeat by Associate
  • 1576 Views
  • 2 replies
  • 0 kudos

STM32F437 Vbat failure detection

Posted on March 16, 2015 at 17:21We are using the internal RTC backed up by a goldcap. In case of a power outage the backup voltage becomes lower by increasing time and at some time the oscillator stops running, but the RAM still remains valid for s...

STM32F4 DMA and ADC

Posted on March 20, 2015 at 00:24Hi,I want to configure the DMA to double buffer mode to work with triple adc in interleaved mode. My idea is to process data while getting new samples from the ADCs.From the examples I've seen I will have no problem ...

pedro by Associate II
  • 3203 Views
  • 9 replies
  • 0 kudos

SDIO on STM32F3-Discovery

Posted on January 20, 2013 at 09:59 Just wondering if anyone has a working implementation on the STM32-F3Discovey of SPI access to a SD card? I'm using stm32303c_eval_spi_sd.c and stm32303c_eval_spi_sd.h fromSTM32F30x_DSP_StdPeriph_Lib_V1.0.0/Utilit...

huberbua by Associate
  • 2330 Views
  • 5 replies
  • 0 kudos

STM32F4 connect to Network printer

Posted on March 29, 2015 at 07:55Dear All,When I enter the IP address of my network printer on web browser, it shows page which contains print counter and more  which I taken prints from the printer. So my project is connect the STM32F4 MCU to netwo...

pic_micro by Associate II
  • 2178 Views
  • 3 replies
  • 0 kudos

STM32F042 USB does not work.

Posted on March 28, 2015 at 19:49Hi, I have an application that works on an STM32F072R. It uses ChibiOS. Then I built a board with an STM32F042F, and now it doesn't work. I thought I could ''test'' the software on the '072, and then deploy on the '4...

Using ch2 and ch4 as input capture

Posted on March 18, 2015 at 13:44 Hello, I'd like to use channel 2 and channel 4 of TIM2 as input capture. Channel 2 work fine, but channel seems returning the timer counter. Here's the code: GPIO_InitTypeDef GPIO_InitStructure; TIM_...

kahseng05 by Associate II
  • 8199 Views
  • 26 replies
  • 0 kudos

STM32F0 LED's Not Running and Cannot Be Connected to PC

Posted on March 28, 2015 at 19:40Hi all,I have an STM32F0R8 board and I am a newbie. I have mistakenly touched 5V and GND pins together while the board connected to my PC. At the same time as the two pins touched, LED's LD1 and LD2 went off. After t...

STM32CubeMX and BUG in LTDC HAL

Posted on March 28, 2015 at 16:00if you need more than the width of the image width of the visible region it is necessary to change the HALDM00031020.pdf16.7.23 LTDC Layerx Color Frame Buffer Length Register (LTDC_LxCFBLR)(where x=1..2)This register...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.