STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32f407 gui on pc via usb

Posted on April 25, 2015 at 16:49Hi, I have made a project and I want to control some parameter's values from my pc's screen using usb communication.. Is there any easy way to make a simple GUI and control these values?PS: I've never made a GUI befo...

zarkscon by Associate II
  • 2273 Views
  • 4 replies
  • 0 kudos

Need help with RS232 receive & STMCubeMx

Posted on August 02, 2014 at 08:45Hi,I'm using RS232 on USART2 of STM32F407 with CubeMx 4.0. I have a protocol which starts with '[' and ends with ']'. I need everythin between 2 braces and I have variable record length. So its not possible to use H...

Osto by Senior
  • 4515 Views
  • 10 replies
  • 0 kudos

Flash page size for STM32F405?

Posted on April 25, 2015 at 03:55What is the page size for flash on the STM32F405 chip?  I can find the layout of the flash in RM0090 manual, but the page size is nowhere to be found.  Is there somewhere else I should be looking?  Surely it's docume...

TDK by Super User
  • 1491 Views
  • 2 replies
  • 0 kudos

Stm32f429 discovery only run at download and debug mode

Posted on April 19, 2015 at 23:45Hello, I'm using IAR and I configured stm32f429 discovery board by STCubeMX and its libraies. It seems to work fine when I run my code with Download and Debug mode. But when I exit debug mode the board stop running ...

Max heap size and allocating memory

Posted on April 24, 2015 at 19:12Hi!I have STM32F407VET6 MCU with 192kB RAM. I need allocate 150kB for storing image after processing data. However I can't allocate such big array. I though I should increase heap size, but I can't increase it more t...

wojdembi by Associate
  • 2826 Views
  • 3 replies
  • 0 kudos

UART receive interrupt

Posted on April 22, 2015 at 19:02I have a board using an STM32F105.  There is a GPS connected to UART4.  I've been trying to get the RXNE interrupt working for a couple of days now, but I must be missing something. The UART seems to be enabled, as I...

Modify the start address 0x800 0000

Posted on June 26, 2012 at 16:26Hi,My microcontroller is a STM32F103CB.I followed the AN2557 to do an IAP in my software. Everything works fine but now I would like to do something like a dual bank features.I can flash two firmwares at two different...

eancelin by Associate II
  • 15720 Views
  • 28 replies
  • 0 kudos

Handling ADC with DMA

Posted on April 24, 2015 at 07:13Hi, I would like to ask how to sample adc values (potentiometer) using DMA interrupt? #adc #dma #stm32f3discovery

kahseng05 by Associate II
  • 1110 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.