STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Unable to get STM32F103ZE chip working

Posted on May 12, 2015 at 18:53Problems getting new STM32 target runningI've developed a project on an STM32F103RB, and am now trying to move it to a F103ZE chip. However I cannot get my code to run.I have changed the linker file to accound for the ...

GregMusic by Associate II
  • 3066 Views
  • 9 replies
  • 0 kudos

STM32F3 & SysTick_Handler(void) :(

Posted on May 13, 2015 at 00:51hiwhen i compli file stm32f3x0.t, i get this error :stm32f30x_it.c(152): error:  #268: declaration may not appear after executable statement in blockthis my code :/**  **************************************************...

Another retarget.c issue

Posted on May 13, 2015 at 10:45 Hi All, I've been working my way through all the retarget.c threads on here and Keil.com today, trying to resolve the old Symbol __stdout multiply defined (by stdio_streams.o and retarget.o) Symbol __stdin multiply de...

jamie23 by Associate II
  • 3097 Views
  • 4 replies
  • 0 kudos

ADC audio sampling circuit

Posted on May 13, 2015 at 16:36Hi I connected audio to ADC and can DSP with success only if the audio is from speaker out. I need to connect audio from a device which outputs 500mvpp. I am using the follow input circuit http://www.frinos.com/adc.png...

sv2agw by Associate II
  • 1243 Views
  • 1 replies
  • 0 kudos

UART FIFO error using DMA with FIFO disabled?

Posted on May 04, 2015 at 21:45 Hi folks, I'm trying to figure out how to resolve this w/out having to abandon DMA. Any suggestions are most appreciated. The problem seems to be provoked by a slightly larger write to the UART (which is...

hbarta2 by Associate III
  • 1094 Views
  • 1 replies
  • 0 kudos

stm32f4 ,i2c and ds1621

Posted on May 12, 2015 at 19:50 I am using an stm32f4 dicovery with a ds16As indicated in the datasheets, i specified the adress as well as the device pins. The problem is that when i run the program ,it seems to be stuck on the the first fla...

d4ng3r09 by Associate II
  • 1475 Views
  • 2 replies
  • 0 kudos

stm32f4 ,i2c and ds1621

Posted on May 13, 2015 at 10:02 I am using an stm32f4 dicovery with a ds16As indicated in the datasheets, i specified the adress as well as the device pins. The problem is that when i run the program ,it seems to be stuck on the the first ...

d4ng3r09 by Associate II
  • 1110 Views
  • 1 replies
  • 0 kudos

STM32Cube F4 V1.5.0 -- usbd_cdc.c, comment error

Posted on May 13, 2015 at 01:18 * @file    usbd_cdc.c  * @author  MCD Application Team  * @version V2.4.0  * @date    28-February-2015Line 658:  * @brief  usbd_audio_DataInshould read:  * @brief  usbd_CDC_DataIn  since this file deals with CDC funct...

mduffy by Associate II
  • 580 Views
  • 0 replies
  • 0 kudos

GPIO actions - is this how people really write code?

Posted on May 12, 2015 at 17:21 After searching for a long time I understood that the only reading materials I can get are the reference manual and the ST library comments - not a lot. I imagine this is the main reason I can't get even simple th...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.