STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HSE oscillator power consumption

Posted on May 22, 2015 at 12:25Hello,I estimate the total power consumption of a device operating from the HSE oscillator. The MCU part number is STM32L152RBT6.I configured the MCU to operate from the MSI oscillator (2.1 MHz). All the GPIO are confi...

Comparator rising/falling edge propagation delay

Posted on May 22, 2015 at 11:17I am using a STM32L152RC microcontroller and have to detect the length of pulses of about 0.7 V and 3 ?s using the COMP2 comparator. At 2.7 V VCC the worst case propagation delay is 2 ?s in fast mode. A minimum delay i...

STM32F100(RBT6): PWM generation with TIM1

Posted on May 24, 2015 at 19:17 Hi Guys, I am very new to the STM32 family and right now I am using a STM32F100 to be able to generate a PWM with TIM1. The end goal is to generate a PWM that can be filtered to show a sinewave so I need v...

awais by Associate
  • 1463 Views
  • 2 replies
  • 0 kudos

problem using SAI block B on STM32F427VIT6 (100 pin LQFP)

Posted on May 24, 2015 at 22:22Hi, I've been trying to use the SD_B output on an STM32F427VIT6 with no success.  This is the 100 pin package.  With typical SAI usage, SAI block B would not be usable since the MCLK, SCLK, and FS pins are on port F, w...

galens by Associate II
  • 1153 Views
  • 2 replies
  • 0 kudos

PWM pin output and document

Posted on May 24, 2015 at 00:50I am new to STM32F030. I am going to use PWMs as the dimming input of LED driver. I have checked DM00088500.pdf, DM00091010.pdf and DM00051352.pdf already. But I still not able to indentify which pins are the output o...

roychen by Associate
  • 887 Views
  • 1 replies
  • 0 kudos

Triggering DMA on a Timer

Posted on September 10, 2013 at 12:08Hi guys, I'm having a few issues setting of a DMA transfer based on a timer and hoping someone might be able to point out where I'm going wrong. I have a timer (timer 2) which is set to 50 Hz and as far as I can ...

VBAT circuit for STM32F429

Posted on May 21, 2015 at 22:20We are using the STM32F429ZIT6 and we need to keep the RTC running when VDD is not present.  Can we hook up a coin-cell battery directly to VBAT, with no switching/monitoring circuit?  Any help would be MUCH appreciate...

gregw by Associate
  • 2672 Views
  • 3 replies
  • 0 kudos

Measure sleep time using DWT SLEEPCNT problems

Posted on May 12, 2015 at 07:56 Hello everyone, I need to measure sleep time of my Cortex-M4 processor (STM32F4xx). I looked at DWT where I also use normal tick counter and I enabled SLEEPCNT counter. However, I noticed that it is 8-bit ...

tm3341 by Associate II
  • 1449 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.