STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32427 with CubeMX

Posted on May 23, 2015 at 11:34I have a board with a 32 bit SRAM and have used CubeMX to configure a 32 bit data bus, a 10 bit Address bus with a Chip select of NE1. Briefly, Cube has produced the MX_FMC_Init(); file with settings as follows:- hsram...

NVIC_ISPR ''set-pending'' bit to force ISR entry

Posted on May 25, 2015 at 03:50 Hi, I'm running some tests on an STM32F072 to verify my understanding of the docs. Apparently I'm missing an important point regarding the NVIC and pending interrupts... I'm single-stepping through the code ...

fenugrec by Associate II
  • 2657 Views
  • 3 replies
  • 0 kudos

CMSIS: DSP Lib - Frequency Bin Example

Posted on May 22, 2015 at 16:18Estimated colleagues, following I explain the strange behavior:     I am working the STM32F407 ARM processor,    compiling with the GNU Tools ARM (4_9-2014q4) ,    use the HAL provided by STM32CubeF4 v1.5.0,    using...

rs2 by Associate II
  • 3678 Views
  • 4 replies
  • 0 kudos

Need help to execute program from SRAM

Posted on May 21, 2015 at 12:39Hi, I want to execute my code from SRAM of STM32F100. I basically want to copy a program from flash to SRAM and execute the program from SRAMPlease help me understand how this can be addressed.Regards Tejas #flash #...

tejas by Associate II
  • 1977 Views
  • 3 replies
  • 0 kudos

STM32L051C6 SPI DMA extra ghost byte

Posted on May 27, 2015 at 15:33Hi, I have discover there is one extra ghost byte is sent in SPI. I have monitor the memory area of DMA TX buffer, the data there is correct, but I will receive one extra byte in the beginning.Here is my code/* Buffers...

scc by Associate
  • 706 Views
  • 0 replies
  • 0 kudos

Start-up time too long

Posted on May 27, 2015 at 09:51Hello there,I've noticed that the in my application the start-up time, i.e. the time from power-up to the first instruction in main() is about 7 to 8 ms. This seems very long to me.I'm using a STM32F103RC and the IAR c...

roman1 by Associate III
  • 7149 Views
  • 8 replies
  • 0 kudos

Access ''MCU device ID code'' on STM32F103

Posted on May 27, 2015 at 03:29Hi, I'm writing a bootloader, and need to determine the device density and flash size. I can read the flash size OK, from memory address 0x1FFFF7E0 However I can't seem to read the ''MCU device ID code'' , which is des...

SPI clock looks to be floating when not driven

Posted on May 27, 2015 at 09:56 Hi, I'm using spi to read and write from an spi flash part, which is working the vast majority of the time. Occasionally I get an incorrect value. Looking at the signals on a logic analyzer the spi clock s...

stenasc by Senior
  • 1438 Views
  • 2 replies
  • 0 kudos

USART Loopback with STM32F107

Posted on May 20, 2015 at 11:35 Hi, I would make a loopback with my board STM3210C using USART2. I use the code /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=https://my.st.com/public/STe2ecommunities/mcu/List...

loic by Associate II
  • 5529 Views
  • 13 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.