STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 I-CODE and D-CODE buses

Posted on June 26, 2015 at 14:40STM32 documentation says that the I-CODE and D-CODE buses are connected to the internal flash memory. The I-CODE bus is used to fetch instructions and the D-CODE bus is used for data access in the code memory region (...

ds1 by Associate II
  • 7249 Views
  • 7 replies
  • 0 kudos

Coverage Analysis STM32F072CBT6TR

Posted on June 29, 2015 at 17:12Hello everyone,I'm using the MCU STM32F072CBT6TR and now I need to make a coverage analysis for this microcontroller but I really don't know where I should start.Do you have some suggestions?Tools, SW etc etc... whate...

luca by Associate II
  • 1627 Views
  • 2 replies
  • 0 kudos

STM32F427 DAC PA4 and PA5 Voltage Spike on Power Down

Posted on June 30, 2015 at 17:03I am using the DAC outputs on PA4 and PA5 of the STM32F427 LQFP 100 pin part. On power down, these pins show a voltage spike in the range of 1-3V and 50-100mS in length. It didn't seem to matter how the pins were conf...

OV7670 and DCMI problem

Posted on July 27, 2014 at 05:18I have been trying to get the OV7670 cam working with STM32F207zg but seems like something is not clear , first i need to know what is the buffer size to set the DMA to when i want to transfer a snapshot from the cam ...

TIM8 Toggle STM32F4

Posted on June 26, 2015 at 12:32 Hi, I'm trying to toggle some pins when timer 8 overflows. The problem I get is that I don´t see the pins toogle but I can see the timer counting on the debugger, so I think I might be missing some ...

pedro by Associate II
  • 1543 Views
  • 3 replies
  • 0 kudos

STM32F4 getting values from buffer

Posted on July 01, 2015 at 18:07 Hi, I wanted to personalize this code I found to fill half a buffer and then process the data while the second half of the buffer continues to fill. To understand how this works I modified the code so it turns on...

fiulala by Associate II
  • 966 Views
  • 2 replies
  • 0 kudos

STM32F103RF Dual Boot Problem

Posted on July 01, 2015 at 16:43 Hi, I am using STM32F103RF (XL density) micro and want to use the flash banks for firmware update. I took ''FLASH\Dual_Boot'' project of STM32F10x_StdPeriphLib as an example. My design is like that: I...

vcelik by Associate II
  • 1108 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.