STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32f4 Discovery EXTI Clear pending bit

Posted on July 20, 2015 at 00:05Hello all,I tried searching for a bit but couldn't find anything pertaining to my question.I'm trying to set up an external interrupt but I don't understand why exactly we clear the pending bit in EXTI->PR and not in ...

Setup a USB module (FT232) with a STM32F103 MCU

Posted on July 16, 2015 at 18:21Hi all, I have a STM32F103VEH MCU which is connected to a FT232 USB module. All pins at the MCU with alternate functions are connected to the corresponding pins at FT232 USB module, which are: PA11 -> USBDM (USB data ...

danesh by Associate II
  • 4316 Views
  • 9 replies
  • 0 kudos

Missing Byte VCP example

Posted on July 07, 2015 at 16:40Hello everyone,I'm facing a problem in which I'm clueless how to solve. Maybe someone can help me out or give me some hints.To the setup:I'm running two STM32, one STM32F0 to communicate via USB with a PC and a STM32F...

p23 by Associate II
  • 1155 Views
  • 1 replies
  • 0 kudos

STM32CubeMX for SW4STM32 : where is c++ compiler ?

Posted on June 07, 2015 at 18:37Hi, I've generated a project with cubeMx for System workbench. Now, I add some c++ classes which does not compile because they are compiled by eclipse with gcc and not g++. Can anyone tell me how to fix this ? I can n...

JulienD by Senior
  • 2508 Views
  • 4 replies
  • 0 kudos

STM32F4xx ''Idle Line'', ''Idle Character'' detection

Posted on July 20, 2015 at 03:10There seems to be an inconsistent usage of the terms ''Idle Line'', and ''Idle Character'' in the STM32F4 reference manual.In my view, I could consider a transmit or receive line that is idle (without a start bit) for...

gahelton1 by Associate III
  • 1308 Views
  • 0 replies
  • 0 kudos

[STM32F0 Nucleo] Developing on Mac OS X

Posted on July 19, 2015 at 23:02Hi,I have a Nucleo Board, STM32F072R8, and I followed thishttps://stm32geek.wordpress.com/2014/10/21/stm32f3discovery-on-mac-os-x-using-eclipse-gcc-arm-and-openocd/ to develop on Mac OS X using Eclipse IDE. Build Proj...

fredvaz7 by Associate
  • 880 Views
  • 0 replies
  • 0 kudos

STM32F7 using the faults

Posted on July 18, 2015 at 23:13Hi,I'm trying to enable the cortex's fault exeptions for my stm32f7 board.Everytime I call   HAL_NVIC_EnableIRQ(UsageFault_IRQn); or try to enable some other Fault I get an Hard Fault.I already tried to access the reg...

Have I blocked my STM32F103 Eval board

Posted on July 19, 2015 at 15:46I have been using the following setup for trying out a few demo programs. I use the jLINK OB. However it appears that I have blocked my STM32 by uploading bad code.Is there some means of resetting the board in the cur...

0690X000006032xQAA.jpg 0690X00000605HzQAI.png

I2C3 configuration

Posted on April 08, 2014 at 20:48Hi I'm working on STM32F401,I configure I2C1 port as an I2C Master at ''init_I2C1(void)'', and I succeed to communicate with the slave side.  Now I'm trying to configure I2C3 port as an I2C Master at ''init_I2C3(void...

gil23 by Associate III
  • 4365 Views
  • 8 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.