STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Triggering One Pulse Mode timers from software

Posted on July 24, 2015 at 11:57I have been playing around with the STM32F407 for a few days now, learning to set up different timer types and connecting them to each other.However, most of the examples regard starting timers from external input.My ...

audun by Associate
  • 844 Views
  • 0 replies
  • 0 kudos

FSMC + ILI9341

Posted on February 12, 2013 at 16:18Hi,I am trying to control an ILI9341 LCD driver using FSMC interface. The CS driver pin is responsable of switching between sending Data or command and I think that I should connect it to one of the FSMC address l...

stm32f4 usb hid

Posted on July 23, 2015 at 12:37i have stm32 discovery board i have problem 1- the usbd_hid_core.c file is for mouse examble only (send report only) 2-i want to usb hid function for receiving  my data(64byte report)  anyone can help me please. i'm...

elec_st by Associate III
  • 794 Views
  • 1 replies
  • 0 kudos

32-bit Timer out of two 16-bit

Posted on July 22, 2015 at 23:24Hi. I have another question... :)I use STM32F103c8 MCU and it has only 16-bit timers. I need a 32-bit timer with high resolution (72 MHz). I made it with connecting two 16-bit timers (one as master, second as slave). ...

matic by Associate III
  • 2493 Views
  • 4 replies
  • 0 kudos

STM32F030K6T6 persistent memory

Posted on July 18, 2015 at 15:11Hi,I would like to know if I can use this MCU in order to store some bytes in persistent memory area. I took a quick look at the datasheet but I did not see anything. Anyone know the best way to save some bytes to be ...

can over run

Posted on July 18, 2015 at 19:02 i using stm23f429 as can controller for servo drive but some time i have over run problem. i check the signals by oscope and understood that , some time fifo of canbx dose not being empty even a can massage trans...

0690X0000060MnCQAU.gif 0690X0000060MnDQAU.gif

STM32F100C8 Unique ID not Unique!

Posted on July 23, 2015 at 15:17Hello!  I have 13  STM32F100C8  and  I see( Keil memory windows )   at  0x1FFFF7e8 ( contiguous12 bytes) very  strange ''so called'' Uniqe Ids - see below.ffff8a07ffffffffffffffff, ffff8807ffffffffffffffff , ffffa007f...

m512781 by Associate II
  • 5038 Views
  • 11 replies
  • 0 kudos

STM32CubeMX 4.9.0 and write protected .ioc

Posted on July 21, 2015 at 17:47Gee whiz! how about popping up an error message if the .ioc file is write protected and the user hits save and then exits!Crap. Good thing my changes were not extensive but highly irritating nonetheless.

hbarta2 by Associate III
  • 1038 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.