STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

IAP for STM32F0 using STM32Cube

Posted on September 02, 2015 at 15:04Hi, I am wondering if there is an example for IAP using cube for STM32F0? I have found an example for STM32F1 and modified it for my board, STM32F070rb nucleo. I can load an application using the iap, but I have ...

seed by Associate III
  • 2350 Views
  • 4 replies
  • 0 kudos

How to Secure FW and keep IAP function

Posted on September 01, 2015 at 05:48Dear Sir:  My project use STM32F427. The project contains bootloader and main application. The bootloader can be used to update the main application.    Now I want to secure the application. I use Jlink secure ch...

Bootloader without pins manipulating / compilation issue

Posted on September 02, 2015 at 13:10 Hello, I am using STM32F401 Nucleo Board. I want go into the bootloader without pins manipulating. According to the many posts, I have seen in the forum. I added this code to my startup_stm32f401xe.s...

tingting by Associate II
  • 1176 Views
  • 2 replies
  • 0 kudos

ADC Dual - Scan - Continuous mode at the same time ??

Posted on September 03, 2015 at 09:18Hi. Does anyone know, if it's possible to use the mentioned combination? I have 8 Channels - 4 on ADC1 and 4 on ADC2. If I have Continuous mose disabled, it works nicely. I make two parallel AD sequences on both ...

matic by Associate III
  • 664 Views
  • 0 replies
  • 0 kudos

STM32L4 OTG_FS_VBUS issues again

Posted on September 01, 2015 at 22:23I am planning to use STM32L4 on a device powered by two alkaline batteries, and I'd like to use USB OTG. After reading the docs, i have came across a few problems:The first problem is the limitation regarding the...

dimitri by Associate II
  • 1547 Views
  • 1 replies
  • 0 kudos

window watchdog in stm32f103

Posted on September 02, 2015 at 22:29hi every one I'm trying to initial stm32f103rbt6's window watchdog with keil cmsis examples, every thing is OK but in reverse direction,i mean it seems external interrupt & wwdg interrupt handlers are act instead...

mhdizgah by Associate II
  • 914 Views
  • 0 replies
  • 0 kudos

Barracuda App Server for 32F746GDISCOVERY

Posted on September 02, 2015 at 21:56Barracuda Application Server Demo for the Discovery Board(32F746GDISCOVERY)The Barracuda Application Server Demo includes a web based code editor, where you can develop your server side web application directly i...

wilfred by Associate
  • 811 Views
  • 0 replies
  • 0 kudos

STM32 SPI Spoiled Bits

Posted on October 06, 2014 at 13:11 Hello, I have a problem trying to communicate with SPI using the STM32 Nucleo. I am using the STM_HAL_Drivers to read data from an Invensense MPU9 When I read values, I sometimes get spoilage of the la...

0901123w by Associate II
  • 3543 Views
  • 12 replies
  • 0 kudos

STM32F4Discovery SPI1 last bit problem

Posted on September 01, 2015 at 10:35Hello,I have a problem  with SPI1 using the STM32F4Discovery. The STM HAL(STM32Cube_FW_F4_V1.5.0 and V1.7.0  ) driver is used. When I use HAL_SPI_Transmit (master mode, bidirectional) last bit in returned byte is...

alevstiv by Associate II
  • 1173 Views
  • 3 replies
  • 0 kudos

How to enable L1 cache on the stm32f746

Posted on September 02, 2015 at 18:32Hello. I want to enable L1 cache on the stm32f746 controller. In examples from STM32CubeF7 i found that memory protection unit enabled at first and then L1 cache. Is it necessary to enable MPU before L1 cache?

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.