STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

curtomizar file .inf

Posted on September 25, 2015 at 16:30Hi, I need customizar the description the file .inf.The file original description is ''DESCRIPTION = ''STMicroelectronics Virtual COM Port''. I need to write ''FCamara'', but when I do upload with description cha...

luscaam by Associate
  • 1689 Views
  • 1 replies
  • 1 kudos

STM32F411RE I2C

Posted on September 25, 2015 at 21:34 Hello, I would like to configure on a stm32f4 the i2c interface, but the programm crashes in the gpio_init when I add the i2c_init line. Does anyone have an idea? int main( int argc, c...

ST-Link VCP drivers

Posted on September 27, 2015 at 01:17Hey all,I don't know if others have experienced this or not, since google did not turn up any good answers.I'm running openstm32 on Win 7 pro, on a brand new machine I got. My target is the F446 Nucleo board, and...

troyerta by Associate II
  • 1250 Views
  • 1 replies
  • 0 kudos

SPI clock frequecy

Posted on September 26, 2015 at 07:30Hi, My device supports max 500khz SPI clock frequency, So how do i configure my STM32F051R8 to support this frequency. #i2c #crosstalk #stm32f0 #spi #uart

Trouble migrating UART USART DMA RX from SPL to HAL

Posted on September 23, 2015 at 21:53I have this SPL project on STM32F427 that I need to migrate to STM32F746. I was hoping I can just program the F7 and it will run but that just shows how naive I am :) Anyway, I wish there was an SPL for the F7 so...

How to compile code into a library for stm32f4

Posted on September 25, 2015 at 17:56 Hello All, Hope you are doing well Clive. Seems like the forums have spam in them ? All those Chinese chars with ''university of xxyy'' stuff ? Anyway I've come back with another question. I have code...

STm wifi module

Posted on March 25, 2014 at 13:24Hi,Anyone of you have worked on WIFI? I need a small help related to that.I need to develop an application that sends and receives some data via usart, cause I need to communicate with a wifi device (i'm using a stm3...

elaroussi by Associate II
  • 5455 Views
  • 10 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.