STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Nucleo board USB and SDIO signal integrity

Posted on August 25, 2015 at 20:45I am thinking of building several ''shields'' with GSM, GPS, LCD, MicroUSB and MicroSD connectors to stack up on the STM32F401 Nucleo board (by the dual row connectors, not Arduino) but i'm worried about the signal ...

STM32f4 different timers

Posted on October 08, 2015 at 17:35 Hi, I'm working with stm32f4-disco. I made a code that works well: the micro waits for an external interrupt, and when receives the interrupt it makes pulses of 40kHz with a duration of 1 ms. Now, I wanted...

fiulala by Associate II
  • 1616 Views
  • 3 replies
  • 0 kudos

Incorrect baudrate with STM32F103 and Smartcard on USART2

Posted on October 07, 2015 at 15:53Hi all, I am using a STM32F103 chip where USART1 and USART2 are connected to Smartcard units. I have tried to communicate to the Smartcard by first sending a reset signal (according to ISO 77816 definition) and the...

danesh by Associate II
  • 1301 Views
  • 2 replies
  • 0 kudos

STM32Cube L4 demos

Posted on October 02, 2015 at 22:06Hi there. Thanks for the STM32Cube software.  I have a Discovery board and would like to try some USB-OTG testing, but there are only USB demo apps for the EVAL board, is it possible to port them so they run on the...

Is this a bug? - STM32L4, HAL, USART DMA handler

Posted on October 02, 2015 at 14:39Using HAL, I have configured DMA1_CH2 and USART3_TX such that once in a while, a block of bytes will be copied from memory to peripheral, in NORMAL, i.e. non-circular mode. Now, my handler, HAL_USART_TxCpltCallback...

8 bits DAC DMA config on STM32F2

Posted on October 04, 2015 at 17:07 Hi all, I am not sure about a DMA config for DAC on STM32F2. Could you please tell me if I made an error using 8bits words with this DMA config? Especially with DAC base address? #define BUFF...

neoirto by Associate II
  • 2072 Views
  • 2 replies
  • 0 kudos

Bug in the STM32F4xx mbed library

Posted on October 08, 2015 at 11:44 Hello. There's an issue in MBED's spi_api.c file. Function void spi_frequency(spi_t *obj, int hz) line baud_rate = __builtin_ffs(divisor) - 1; The problem is this line makes a...

vech2001 by Associate II
  • 1447 Views
  • 1 replies
  • 0 kudos

Nucleo-L053R8

Posted on August 11, 2015 at 12:00Hello,I'm using nucleo-l053r8 for my project. I have to make a data logger application with a sensor. Here i have developed my code in mbed tool. I also store the values in SD card. Now my task is to make my own cus...

gandhi by Associate II
  • 3501 Views
  • 9 replies
  • 0 kudos

STM32F3 stop mode problem (WFE)

Posted on January 30, 2013 at 15:17Hi, we have a problem with the STOP mode of the STM32F3. We have the feeling, that the F3 immediately returns from STOP mode, if ANY interrupt is enabled and has been activated before entering the STOP mode. The se...

arnold2 by Associate II
  • 9761 Views
  • 16 replies
  • 0 kudos

STM32L053 Standard Peripheral Library

Posted on April 24, 2014 at 11:34Hi All, I am designing the Heat Meter with STM32L053 now. So have you released STM32L053 Standard Peripheral Library yet please? It is very important to speed up our design schedule. Thanks. #stm32l053

alfred by Associate
  • 2842 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.