STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HAL_SPI_TransmitReceive_DMA into EXTI0 ISR

Posted on October 23, 2015 at 02:42 I have a SPI ADC conected to a STM32F4 I'm trying to use it with SPI DMA and DataReady signal with interrupt. This code works fine: while(1) { //PB0 = DRDY from ADC if ( (HAL_GPIO_ReadPin(GPIOB,...

SPI DMA with HAL (STM32F4Disco)

Posted on October 17, 2015 at 11:07 I am currently trying to make DMA periodically pull data from memory (array ''buffer'') and push it to spi. When I manually call the SPI_Transmit function, it transmits something, the clock line shows up on my...

Leonelf by Associate II
  • 1021 Views
  • 1 replies
  • 0 kudos

STM32F3 I2C LSM303DLHC Hangs I2C_ISR_TC

Posted on October 22, 2015 at 21:55 Hi everyone. I must ask for help one more time. I've been tring do it on my own (using examples and my own functions), but nothing works. I'm want to read data from ACC, just one register, on my F3 disco...

HAL ADC + DMA increment memory

Posted on October 20, 2015 at 12:07Hello there,Looking at the example ADC_RegularConversion_DMA I am trying to obtain this functionality:Using DMA conversion is started in circle (never stoping) each time the conversion is finished it should put the...

NOR memory internal address

Posted on October 22, 2015 at 11:47Hello,I would like to program an external flash (S29GL128S10) connected to the STM32F429 at address 0x64000000  using the ST-LINK Utility. I didn't find an external Loader for this need so I am trying to create it ...

STMStudio and STLink-V2.1

Posted on October 22, 2015 at 10:58Hello, STMStudio seems to have not received any update since last year and so does not support STLink-V2.1. Is support for STLink V2.1 planned or is STMStudio EOL?

STM32 USB OTG and uc20

Posted on October 20, 2015 at 10:18HiI use stm32f429-discovery board. I want to use uc20  (GPS/GPRS) module.uc20 has usb interface. I want to connect uc20 to stm32f429 with usb interface. I dont now how to develop driver.also uc20 has multi interfac...

DMA only sending one byte and not whole buffer

Posted on October 21, 2015 at 14:43 STM32f30x The aim is to trigger the DMA from a timer. The DMA should then send one row of data from my buffer to the SPI. The DMA should then trigger an interrupt which points DMA to the next row in the bu...

JustMe by Associate III
  • 5521 Views
  • 9 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.