STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Main clock + Simulation EEPROM

Posted on November 04, 2015 at 08:38Hi,I just started to pickup programming STM32F0308-DISCO based on STM32F030R8T6.I have configurated the clocks and got the timers working on the desired 48 MHz. But when I try to simulate a delay with a for loop i...

Birdo by Associate II
  • 1693 Views
  • 3 replies
  • 0 kudos

STM32F407IG Ground pins

Posted on November 04, 2015 at 13:14In document DocID022152 Rev 5, pinouts , Figure 16 (STM32F40x UFBGA176 ballout)- all the pins in lines F6-F10...K6-K10 is marked as VSS. But, in the following pinouts table, Table 7 (TM32F40x pin and ball definiti...

shlomo by Associate II
  • 1307 Views
  • 4 replies
  • 0 kudos

STM32F469I-Discovery demo does not compile

Posted on November 04, 2015 at 21:28 Hi! I've just got my STM32F469I-Discovery board. I'm trying to compile the provided demonstration example, but I got the following Errors. *** Using Compiler 'V5.06 update 1 (build 61)', fo...

gergely by Associate II
  • 3364 Views
  • 5 replies
  • 0 kudos

STM32F469I-Discovery demo does not compile

Posted on November 04, 2015 at 20:27 Hi! I've just got my STM32F469I-Discovery board. I'm trying to compile the provided demonstration example, but I got the following Errors. *** Using Compiler 'V5.06 update 1 (build 61)', fo...

gergely by Associate II
  • 1035 Views
  • 1 replies
  • 0 kudos

STM32F4-Discovery Lowest Possible Power?

Posted on November 03, 2015 at 20:44I am fully aware of the SM32F407's low-power capabilities.  What I was wondering is what are the EVAL kit's low-power capabilities?  It seems no matter which mode the MCU is in, I'm forced into drawing ~40mA.  It'...

shawn2 by Associate II
  • 1096 Views
  • 2 replies
  • 0 kudos

How to use Zones in Touch Sensing Library STM32L053

Posted on October 25, 2015 at 12:00Hello, I'm currently working on a project where I have 8 touchkeys @ 3 banks.This is working just fine. But to speed up my prox detection (wake up) of a device I would like to add one more bank (where all channels ...

purkovic by Associate II
  • 1157 Views
  • 1 replies
  • 0 kudos

I2S clock frequency problem

Posted on February 07, 2014 at 08:24Hi,I am interfacing TLV320AIC3204 to stm32f415, at this stage i am able to configure codec IC using I2C successfully and also able to operate I2S interface in full duplex mode with DMA on both transmission and rec...

usama by Associate II
  • 2578 Views
  • 3 replies
  • 0 kudos

Cube STM32F411RE Demo - SPI CRC Calculation?

Posted on November 04, 2015 at 05:27Started using the Cube/HAL libraries and working with the F411RE demonstration with the Adafruit 1.8'' TFT shield.  It has a SD card slot on it and uses it to load images onto the display.  Not sure if ST doesn't ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.