STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 ADC DMA Overrun problem

Posted on December 03, 2015 at 12:57I have been struggling on this over the past few days and its starting to really push my buttons now.Device: sTM32F405RGTXBasically I have ADC 1 configured in regular mode Channel 10 and 11, and I am using DMA to ...

help - how to protect STM32 analog inputs ?

Posted on December 02, 2015 at 14:17hello dear forum,I need protect the analog inputs of my STM32 becouse I measure the output of a current detectorand STM32 GND is the same with the GND of power circuitand I face problems with analog inputshow can ...

STM32L152 comparator triggers timer

Posted on November 12, 2015 at 11:30Is it possible to trigger any timer by comparator output in stm32l152? I want to configure timer to one pulse mode and i want to trigger it by comparator output. I have studied manual carefully, but I still don't ...

SPWF01SA SSL Library

Posted on November 27, 2015 at 16:46Hi. I want to know which SSL library is integrated in SPWF01SA (it is WiFi module)? In the feature list is written that SSL/TLS 1.2 is supported but I need to know the specific library inside. Also, is it possible...

ta by Associate II
  • 946 Views
  • 1 replies
  • 0 kudos

STM32F3 GPIO current sourcing question

Posted on November 30, 2015 at 10:52Hi, I am using STM32F301. If I configure the GPIO pin to be output mode, and configure it to be open-drain with pull up, what would be the pin's current sourcing capability? What is the value of the internal pull-...

song by Associate II
  • 996 Views
  • 1 replies
  • 0 kudos

CIFS/SMB Library for embedded systems

Posted on October 21, 2015 at 16:45Hi! I'm wanting to connect my STM32 board to my network and be able to access files on my local network share. Does anyone know of a SMB/CIFS library for embedded systems that I could use? Cheers!

STM32F0 Timers

Posted on December 02, 2015 at 00:56I am having trouble creating a PWM output using a timer (timer 3, channel 1). Processor is an STM32F072CB. I'm using the following code: Note: GPIO clock is enabled for port A   RCC_TypeDef  *rccptr = RCC;   // En...

greenk by Associate
  • 1553 Views
  • 2 replies
  • 0 kudos

STM32F7 Questions regarding code and performance

Posted on December 02, 2015 at 08:20 Hello. I have very DSP load program to run, and STM32F4 is not up to the task, so i switched to STM32F7 and HAL ( it is just asking for trouble ) I have few question related to code execution from...

I2C setup with Hal libraries

Posted on December 02, 2015 at 15:03 Hello everyone, I am new to this forum and to ST microcontrollers and need some help.. Trying to inialize and pick the right functions for Read and Write from the cube(HAL) libraries, to connect with an...

td by Associate II
  • 1028 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.