STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Strange CUBE USB device driver behaviour

Posted on December 04, 2015 at 13:27Hello, I work with STM32F429-Disco. I have problem understanding how USB class device driver should be implemented. From MSC class driver implementation I see: - DataOut is called for ep out where Receive() is cal...

0x4e71 by Associate II
  • 1034 Views
  • 1 replies
  • 0 kudos

strange problem

Posted on December 10, 2015 at 14:11Hi i have a strange problem. i have configured the spi6 on stm32f429 board and i have included the configuration below. After i download to flash, its starts blinking the lights.i am not understanding why the led ...

arunease by Associate II
  • 1403 Views
  • 7 replies
  • 0 kudos

CAN on STM32F756xx

Posted on December 10, 2015 at 16:12Hello,I try to send CAN frame from CAN1 to CAN2 on STM32F756xx. CAN1 works in a master mode and CAN2 in a slave mode.I can transmit frames from CAN1 as well as from CAN2 but I can't receive any messages.Also when ...

can't find COM port on my PC.. (STM32F401RE board)

Posted on December 08, 2015 at 08:39Hi, I've been seeing COM2:STMicro... port on my PC but after I removed some drivers and installed some, it disappeared. Still I can connect to the target using ST-LINK/V2-1 utility and I can debug the code using u...

ckim by Associate II
  • 3549 Views
  • 3 replies
  • 0 kudos

STM32F4 slave uart DMA circular buffer

Posted on June 09, 2014 at 19:00I have to write new driver for uart slave interface with a STM32F407 For RX I thought I enable DMA in circular buffer  mode. The device is always ready to receive and with HC and TC DMA interrupt I can download the R...

Device identification

Posted on December 10, 2015 at 20:42Hi, short question, what is the meaning of the last two characters (T7) of device ID STM32F407VGT7? Thanks.

paul2 by Senior
  • 696 Views
  • 1 replies
  • 0 kudos

stm32F746 and I2C

Posted on December 07, 2015 at 22:40Hi,Just need some help with the I2C peripheral of the 32f7. I would like to read 2 bytes from an imager Aptina. The i2c sequence is composed of 1 write cycle followed by 2 read cycles. After the write, the stop ha...

Counting pulses over a certain time period

Posted on November 30, 2015 at 17:00Hi, I am using STM32F1 and want to count the number of times a digital input is high, over a period of 5 seconds. Can anyone please help me with this query? Thanks in advance.

llmg343 by Associate II
  • 2240 Views
  • 5 replies
  • 0 kudos

STM32 UART reliability with high baud rate

Posted on December 08, 2015 at 17:32Hello everybody,I posted a http://electronics.stackexchange.com/questions/204376/stm32-uart-reliability-with-high-baud-rate recently on stackexchange, but didn't get satisfying answer. It's related to reliability ...

jalooc by Associate
  • 4138 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.