STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

WFI hardfault on wakeup

Posted on September 29, 2014 at 02:28Hello everyone:Here is my problem.I am using the STM32L152. When I execute the WFI instruction, the processor goes to sleep just fine. However, when it wakes up from an external interrupt line, the processor imme...

cmurp77 by Associate III
  • 5315 Views
  • 18 replies
  • 1 kudos

STM32F103 Supply Problem

Posted on January 12, 2016 at 15:40Hi,First of all sorry for bad English.I had designed a PCB for STM32F103 micro-controller for my specific job. The thing is micro-controller works fine when J-link is connected. J-link programmed micro with no erro...

amin by Associate
  • 2922 Views
  • 5 replies
  • 0 kudos

Code in CCM RAM

Posted on January 09, 2016 at 20:36Hi.I tried to put code in a CCM RAM (STM32F303) as described in AN4296 and I was very impressed. It was more than 30% faster, than if the code is in flash.Mentioned PDF (AN4296) says that it is not recommended to p...

matic by Associate III
  • 6039 Views
  • 14 replies
  • 0 kudos

Let's Decode some ADC+DMA output

Posted on January 08, 2016 at 19:21  The original post was too long to process during our migration. Please click on the attachment to read the original post.

troyerta by Associate II
  • 4526 Views
  • 8 replies
  • 0 kudos

STM32F0 SPI Slave wrong behaviour

Posted on January 08, 2016 at 15:28Hi I'm stuck in my project by this spi problem. What i do is simple, i send a data from a stm32f0 (master) to another one (slave) but here is the problem: while i see on the scope the good frame, the slave device d...

STM32F072 usart doesn't reveive data

Posted on January 11, 2016 at 16:44 Hi,i am working with Stm32f072 microcontroller and i can send datasuccessful.But my code doesn't enter usart interrupt.My code is below,thanks for your support. void USART_Configuration() { GPIO_InitTyp...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.