STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

PWM output without using Timer as AF.

Posted on February 10, 2016 at 15:02I want to generate a PWM output for a GPIO pin without using Timer as the AF. Is there any other way of accurately doing this? Timers in other modes can be used. Code samples will be helpful. #output #pwm #disc...

STM32F373 SDADC Calibration hardfault

Posted on October 03, 2014 at 09:45Hello, I would like to kindly ask for a help with calibration of SDADC peripheral on chip STM32F373. Im using SDADC with TIM19 triggered conversions 1000Hz.  I have tried two variants of calibration A)     /* Set C...

ssubrt9 by Associate
  • 1174 Views
  • 1 replies
  • 0 kudos

Programming STM32F429I Discovery Board Error

Posted on February 10, 2016 at 10:46Hi allI am using STMF429I Discovery Board. I am Using Keil V5. I have downloaded and Pack for STM32F429ZITx 2.7.0(2015-12-08_ DFP, Installed added ST- Link Utility and updated ST-Link firmware to V2J24S0.. I did a...

Edge Triggered Interrupt Functionality on EXTI15_10_IRQ

Posted on February 09, 2016 at 23:36Hello: What I am trying to do seems pretty straightforward, but the results I am getting don't agree with that. I have 17.5KHz clock that bursts about 7 times/second. I have the interrupt set for rising edge. When...

Return from Exception Handler

Posted on February 10, 2016 at 13:21Hi,I am using STM32F439 Eval board. I am trying to understand Micro. supported exceptions. I want to know, Is there anyway to come back to normal operation once we get any exception.lets assume i am doing division...

pratik by Associate
  • 1188 Views
  • 1 replies
  • 0 kudos

DSP Library issue

Posted on February 10, 2016 at 13:21Hi, I am trying to do FFT using stm32f4 discovery board. I am using CooCox CoIDE. After adding DSP Libraries and everything I am getting this problem during Compile.[cc] arm-none-eabi-gcc -mcpu=cortex-m4 -mfpu=fpv...

uart hal library

Posted on December 21, 2014 at 00:23 Hello, It seems keil is forcing me to use the hal libraries and i'm triying to work with them. i've spent hours triying to make an uart com work. i've tried the example from the STM32cube_F4 ...

jdpv by Associate II
  • 2002 Views
  • 2 replies
  • 0 kudos

I2S2(I2S2_ext) full duplex on STM32F301x6

Posted on February 08, 2016 at 14:52Hello! I want to use I2S2(I2S2_ext) in full duplex mode. I configure I2S2 as slave TX and I2S2_ext as slave RX. Will it work ? Or I2S2 must be master only ? Thanks in advance!

korhal by Associate II
  • 1683 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.