STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FMC SRAM - Initialization parameter

Posted on March 03, 2016 at 15:36 Hello ST-community, I am able to setup my external SRAM and access and test (memtest) its memory regions. It works! However, I do not know if my configurations are correct. It is hard for me to und...

Input resistors on 5V-tolerant I/O

Posted on February 25, 2016 at 16:07Hi, I'm quite confused about 5V-tolerant input pins of STM32F405. Referring to the manual, the picture ''Basic structure of a five-volt tolerant I/O port bit'' shows diodes that protect the port. In this configura...

francesco by Associate II
  • 1846 Views
  • 2 replies
  • 0 kudos

stm32f407 EXTI interruption freeze

Posted on March 01, 2016 at 12:11Hi all,Trying to implement a basic external interruption on the stm32f407 discovery board, the microcontroller allways freeze after receiving external interrupt. After some test i discover interrupt cause a call to t...

STM32F103 64 pin package. Vref questions

Posted on March 02, 2016 at 18:12Folks, The 64 pin package of the STM32F103 has no Vref pins. I can't see any way, though, of switching between external and internal ref for *any* of the parts. I'm assuming that where there is no Vref pin, you can ...

DiBosco by Senior II
  • 2411 Views
  • 4 replies
  • 0 kudos

SPI NSS configuration

Posted on July 02, 2014 at 15:16Hello, Please could someone post the details to manage the SPI NSS signal? The master drives it ''manually'' using a GPIO bit. I want to use the SPI as a full-duplex master (sending and receiving data simultaneously)....

maximum frequency of STM32F0 @2,5v

Posted on February 29, 2016 at 15:57Hi, What is the maximum frequency of STM32F030F4P6 at 2,5V ?Does the supply voltage have an impact on choice of capacitor value ?I'm planning to use 20pf capacitors and 8 mhz crystal On the STM32F0 discovery schem...

all by Associate II
  • 2391 Views
  • 5 replies
  • 0 kudos

This can be realized with DAC and ADC in STM32F103?

Posted on March 01, 2016 at 16:52 DAC is used for generating sinus wave 1kHz. 1000 sample is over DMA transferred on DAC 1MHz/1000SPS = 1kHz It would be good to start each sinusoid nullify one of the counters. This signal, after passing through som...

0690X00000605JsQAI.png
wc40 by Associate II
  • 2218 Views
  • 5 replies
  • 0 kudos

Discover Wi-Fi with stm32f407 UART Problem

Posted on February 24, 2016 at 11:12I have difficulty handling Discover Wi-Fi. Currently, I am using keil vision and stm32f407 as a host mcu device Also, I am trying to modify the example code but it is not working well. I need help and advice. In t...

manjae by Associate II
  • 4156 Views
  • 11 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.