STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32f0 can't enter hardfault

Posted on February 26, 2016 at 18:26Helloabout 'bkpt' instruction and no debugger attached? ( semihosting problem)I read that must be generated HardFault exception in this case but this never happens.I have already tested HardFault vector with divid...

harryzz by Associate
  • 1472 Views
  • 2 replies
  • 0 kudos

I don't know why STM32F427 I2C3 will send the byte repeat?

Posted on March 04, 2016 at 17:38Hi all,Are there have any one know this problem, I have to trying send only one byte via I2C3, butI don't know why STM32F427 I2C3 will send the byte repeat? uint32_t I2C_WrBuf(I2C_TypeDef* I2Cx, uint8_t DevAddr, uint...

0690X00000605N4QAI.png

Sin wave generation problem using TIM1 & PWM

Posted on March 02, 2016 at 23:17I am a student from University of Cairo Iam trying to  generate a 50 hz sinusoidal using my stm32f4 discovery board. I am running my timer in 10khz (switching freq = 10khz) and I am using a lookup table (generated fr...

ralph by Associate II
  • 5246 Views
  • 7 replies
  • 0 kudos

Nucleo STM32F401 testing HAL SPI driver

Posted on March 04, 2016 at 23:47Hi, i wrote a simple program in Keil uVision to test the HAL SPI driverThe logic analyzer shows that there is clock activity as expected but the MOSI ouput stay low all time even with pull-up enabled (see attached sc...

USB CDC problem

Posted on March 02, 2016 at 00:07I am using the Stm32CubeL4 to generate a USB device with a CDC class. This is on a custom board. I am not using the USB ID line or VBUS. It runs, but USBD_CDC_Init() is never called. On the Windows side, I see an ''...

jstefan by Associate
  • 1224 Views
  • 1 replies
  • 0 kudos

STM32 F4 discovery USB audio program

Posted on March 04, 2016 at 21:12Hi All,I am now trying to building a USB sound card with microphone.When I use USBlyzer to monitor the usb communication, it didn't have ''set configuration'' and start fails.which part is wrong?Thanks.

fangdu by Associate II
  • 837 Views
  • 0 replies
  • 0 kudos

512kB chip won't flash, but 2MB will (f429)

Posted on March 04, 2016 at 06:47I'm developing an application using the stm32f429 and have completed the firmware. The total size is only ~300kB so I'm trying to downgrade to the 'VE' version with only 512kb as it's substantially cheaper.On my prot...

STM32F0 Hard Fault Error

Posted on March 02, 2016 at 16:40Hi all,The issue that I am having is that I having is last night I was programming and found that my code suddenly stopped functioning completely. After running in debug mode I found that the code immediately enters ...

eric5709 by Associate II
  • 3514 Views
  • 6 replies
  • 0 kudos

Cannot flash STM32F103 if PLL enabled

Posted on February 26, 2016 at 02:55I'm trying to deal with the setting clocking of STM32F103 MCU without the use of third-party libraries.I wrote several functions for this: http://pastebin.com/kLQS9UmwIf I setup clocking by stm32_rccUseHSE, then e...

kiv by Associate II
  • 2215 Views
  • 4 replies
  • 0 kudos

External oscillator use in STM32F103xxx

Posted on March 04, 2016 at 18:00Can I use an external oscillator module to drive a clock directly into the 'oscillator in' pin?ST documentation only shows crystal with load capacitors. #stm32 #oscillator #-

cgordon by Associate
  • 1167 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.