STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F7: CAN2 Wrong Filter ID (FMI)

Posted on July 25, 2016 at 16:20Hello all,I am using both CAN on my device.  It is all working well except that I am receiving in HAL_CAN_RxCpltCallback() an incorrect ID value for all my CAN2 filters.  I have 6 filters on CAN1 from 0 to 5 and 6 fil...

keaven by Associate II
  • 1132 Views
  • 1 replies
  • 0 kudos

How can I have 4MHz I2C signal ?

Posted on July 25, 2016 at 03:50I know that I2C's official speed is 100KHz (Standard Mode), 400KHz (Fast Mode), 1MHz (Fast Mode Plus).But, in my lab application, I need to implement 4MHz I2C signal. I had used FPGA logics to achieve 4MHz I2C signal....

taz1000 by Associate III
  • 978 Views
  • 1 replies
  • 0 kudos

UART under noise: data still usable?

Posted on July 25, 2016 at 14:46Hello, I'm trying to find out how UART received data is influenced by noise. STM32F1xx reference manual states that the UART will check three sampled values from the middle of each bit. If one of those three values di...

Automotive application (Engine Control Unit)

Posted on July 25, 2016 at 14:15Hello, STM32F0 are my favourite ARM based 32bit MCU. Now I have a design of disel engine control unit for cars and gensets. So we need automotive grade MCU. I am trying hard to find one. But I think not available from...

UART with DMA mode

Posted on June 16, 2012 at 15:32hi everyoneneed help regarding UART with DMA mode,i am using STM32F407 Discovery Board,i want to configure UART4 with DMA, and want it to generate interrupt when DMA completes filling the memory. so should i configure...

muhammad by Associate II
  • 19762 Views
  • 22 replies
  • 0 kudos

LWIP send data

Posted on March 18, 2014 at 20:08 Hi, I use LWIP and FreeRTOS like WEB server. It's OK. But now, I want send data to otger page for example by GET. Like this: http://www.page.com/p.php?json=1234 Can you help me please? Here is my co...

zavodny by Associate II
  • 8317 Views
  • 18 replies
  • 0 kudos

UART PRBLEM with STM32F3

Posted on January 30, 2014 at 10:51The original post was too long to process during our migration. Please click on the attachment to read the original post.

hilwan by Associate II
  • 7502 Views
  • 21 replies
  • 0 kudos

ADC noise and source impedance

Posted on July 23, 2016 at 02:50Does STM32F103RB use switched capacitor ADC circuit which produces some noise in the process and requiring source impedance to be 'not too high' or else accuracy will degrade?  The signal is single channel and no MUX...

john1389 by Associate II
  • 1118 Views
  • 1 replies
  • 0 kudos

ADC noise STM32F103RB

Posted on July 23, 2016 at 02:44What configuration parameters (clock freq, sampling clock count, etc.) can I tune in order to minimize ADC reading noise when sensing a relatively low speed signal?  I am currently getting about 10 to 20 LSB differe...

john1389 by Associate II
  • 1163 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.