STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Where can I find USB Full Speed Device Library for STM32F4?

Posted on August 04, 2016 at 18:22I could find the STM32F0x2_USB-FS-Device_Lib V1.0.0 for the STM32F0 but I can seem to find the equivalent USB Device library for STM32F4. Does anyone happen to have the link? I have downloaded the ''en.stm32cubef4''...

Vu.Andy by Associate III
  • 1377 Views
  • 3 replies
  • 0 kudos

USBD_HID_Init

Posted on August 05, 2016 at 02:33I have an STM32F416 embedded in a USB device that I want to act like a keyboard device when plugged in to a PC.  I'm using the STM32Cube USB device library and the UM1734 documentation.  In the documentation it says...

ron2399 by Associate II
  • 1367 Views
  • 1 replies
  • 0 kudos

Bug with STM32F7 HAL UART Tx DMA

Posted on March 21, 2016 at 20:10 Hello, I'm currently running on the STM32F746VG, and used CubeMX to generate the configuration code for a simple USART Tx Output using the DMA. When callingHAL_UART_Transmit_DMA(..) it would transm...

Hard Fault in STM32CubeMX Generated Code

Posted on August 05, 2016 at 06:07This is an STM32CubeMX 4.16.0 generated project. The  STM32CubeMX project file is attached. The processor is an STM32F373VCT6 I have a Hard Fault. Below is the call stack and register contents when the Hard Fault ha...

spflanze by Associate II
  • 3055 Views
  • 1 replies
  • 0 kudos

ITM configuration for SWD print

Posted on July 25, 2016 at 08:42Hello, We are using STM32l476 uC with Jlink segger debugger, and trying to print logs through ITM to Segger J-Link SWO Viewer , the 48 MHz HSE clock is being used as sysclk with RCC_PLL_NONE, We are using   ITM_SendCh...

Difference between STM32F429i-DISCO & STM32F429i-DISC1

Posted on August 04, 2016 at 14:50Hi y'alldoes any one know the difference between STM32F429i-DISCO & STM32F429i-DISC1 that may be causing the issue I have & how to get around it ?basically I've been using a STM32F429i-DISCO to build a demo unit for...

daemynnur by Associate II
  • 3316 Views
  • 6 replies
  • 0 kudos

FMC NAND problem

Posted on August 05, 2016 at 12:06Hi, I have a problem when you use the microcontroller STM32F746(NUCLEO-F746ZG)   FMC together with the NAND memory K9F1G08U0E. The documentation states that it is sufficient to read the data at the address 0x8000000...

Konmax by Associate II
  • 764 Views
  • 1 replies
  • 0 kudos

STM32L476VGT6 pin PC13 odd behaviour

Posted on August 05, 2016 at 00:16We have had an odd problem with using pin PC13 as an output GPIO (for active-low chip-select of a bit-banged SPI).  (PC13 is not defined as a GPIO_EXTI13.)  We found that controlling this GPIO somehow leads to USB (...

timers clock divider on STM32f103

Posted on August 05, 2016 at 10:53hi,I just found that clock devider not work for some Frequency, for example if PLL is used without divider, Timer clock cant be devided. EnjoyAll the best, #stm32 #timer #interrupt

miroslav by Associate III
  • 690 Views
  • 0 replies
  • 0 kudos

STM32F746, ADC

Posted on August 03, 2016 at 08:43Hello, can someone to explain to me what happen when you use 8 channels on ADC, and use DMA. How DMA take ready sample from data register. I think when first channel is ready, dma take it first, after that second, t...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.