STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F103 Sweep frequency

Posted on August 05, 2016 at 07:50 Hi im newbie with this mcu, and im try to doing a sweep of frequency with TIM3 and the chanel1, A6. my main code its the next while (1) { unsigned int i=0, j=0, h=0; for(i = FrequencyStart; i < (Frequenc...

0690X00000602rDQAQ.jpg 0690X00000603AhQAI.jpg
woutnme by Associate II
  • 1290 Views
  • 1 replies
  • 0 kudos

Byuing evaluation tools from ST.

Posted on August 07, 2016 at 14:35I can not find any information about valid payment types and if  shipping is included.I like to use paypal for Internet payment.Can anyone enlighten me ?

itchef by Associate
  • 1187 Views
  • 1 replies
  • 0 kudos

STM32F407VGT6 programming and debugging

Posted on June 30, 2016 at 22:25Hello, I have developed my code using IAR workbench, tried it on STM32F4 discovery board and it worked well. Now I want to download the code on STM32F407VGT6 chip I bought from digikey.com directly without the develop...

I2C Problem - STM32F4 DISCOVERY

Posted on August 03, 2016 at 08:33Hello everyone. I have searched the forums but could not figure this out.I am using the STM32 F4 Discovery, AC6 (System Workbench), and the standard peripheral libraries.On the Discovery Kit PA8 (pin 100) should be ...

Timer Interrupt Callback

Posted on July 05, 2016 at 18:15In Hal Library version 1.5.1 hal_timebase_tim.c the HAL_TIM_PeriodElapsedCallback(htim) increments uwTick. That's OK for TIM6, since it is now dedicated to that function, but other timer update interrupts also call th...

thumb misalignment? [was: memcpy oddness]

Posted on August 03, 2016 at 05:47 Hi Guys, I've recently started working with the STM32F0 series of microcontrollers, took a while to get a fully functional build chain up and running, but now everything looks good on that front. ...

morgan by Associate II
  • 2068 Views
  • 5 replies
  • 0 kudos

STM32F103 issues with ADC1 6 channel DMA transfer

Posted on August 06, 2016 at 17:38 Hello, I have used ADC1 in 4 channel mode successfully in my project with DMA1 transferring the values in circular mode. Now I needed to add 2 more channels, but for some reason as a result reason the ch...

lkaino by Associate II
  • 899 Views
  • 1 replies
  • 0 kudos

[STM32F103] USART1 TX DMA only fires once

Posted on August 06, 2016 at 15:06 I have a problem, I wrote some code based of https://github.com/g4lvanix/STM32F1-workarea/tree/master/Project/STM32F10x_StdPeriph_Examples/USART/DMA_Polling and it only fires the USART1 TX DMA once for some rea...

zhausq by Associate III
  • 1957 Views
  • 4 replies
  • 0 kudos

How to get debug output from NUCLEO F091RC

Posted on August 06, 2016 at 20:11I'm used mbed.  How can I get printf or debug message output? Does mbed have a way to get printf direct from Nucleo's USB port?Or, must I use Nucleo's STLINK RX/TX and to serial/USB cable, to Windows-7 terminal emul...

doug by Associate
  • 962 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.