STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CAN filters

Posted on May 11, 2012 at 08:03Hello everyone! Can anybody help me to understand the following thing about filters in CAN for stm32f10x. 1) Can I configure filters for receiving only messages with the specific range of ID values. For example, I want...

STM32F767ZI Hard fault when using ITCM RAM

Posted on August 30, 2016 at 19:05I am playing with the ITCM RAM on a Nucleo-144 board. I am having problems with the ITCM RAM causing a hard fault when I call a subroutine from inside a subroutine. I have successfully used the ITCM RAM to store a f...

STM32F100RBT6B l293d 28byj-48

Posted on August 29, 2016 at 13:08 Hello i am trying to launch simple stepper ( http://robocraft.ru/files/datasheet/28BYJ-pdf) using l293d. Connecting 28byj-48 to the L293D: Engine contact 1 is connected to the output 1. E...

anton23 by Associate II
  • 1067 Views
  • 1 replies
  • 0 kudos

SDADC and ADC Calibration Time Interval

Posted on August 29, 2016 at 22:44If a processor is to be run continuously for weeks, months, even a year or more is it sufficient to calibrate the SDADC and ADC once at power up, or would there be a benefit to calibrating at regular time intervals?...

spflanze by Associate II
  • 2124 Views
  • 2 replies
  • 0 kudos

isochronous assynchronous transfer troubles

Posted on August 30, 2016 at 17:21Hello, i'm having big troubles with isochronous assynchronous data transfer with feedback. Have spent weeks on the subject, and its all mess in my head now, because simple things who are supposed to work, doesn't, a...

STM32 interfacing RF module (TI CC11xx) over SPI

Posted on August 25, 2016 at 17:20Hi,has anyone worked with on of the TI CC11xx RF modules?I have searched a lot to find STM32 related code examples, but with no success. All I found is the following discussion, where someone is also using CC1101 RF...

vojislav by Associate
  • 2706 Views
  • 2 replies
  • 0 kudos

STM3240G-EVAL TS472 audio preamp driver?

Posted on August 14, 2016 at 16:11Hi there,I see that inside this board there is TS472 audio preamplifier, but there is no driver for that.preamp is connected to pin PF10 (ADC3_IN8).PAGE 50/67:http://www.st.com/content/ccc/resource/technical/documen...

hitsumen by Associate II
  • 1026 Views
  • 1 replies
  • 0 kudos

Beginner question on what constitutes a device USB interface

Posted on August 24, 2016 at 18:00Been reading through the USB document and going through the codes but still having a bit of trouble grasping the concept of an interface. What would constitute an ''interface''?  Does it encapsulate a class with the...

Vu.Andy by Associate III
  • 747 Views
  • 1 replies
  • 0 kudos

STM32F7 fast threshold implimintation

Posted on August 25, 2016 at 10:39Hi,I have a 800 bytes array and I need to check if each byte is bigger than a threshold valuefor (i=0;i<800;i++) if Data[i] > TH then ....is there any other method to implement this threshold without loop and if?Tha...

priven by Associate II
  • 945 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.