STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L0 with BM70 bluetooth

Posted on September 05, 2016 at 15:15  The original post was too long to process during our migration. Please click on the attachment to read the original post.

ibrahim by Associate II
  • 1089 Views
  • 0 replies
  • 0 kudos

Bad Phy strap values captured on Nucleo144 boards

Posted on September 02, 2016 at 13:40On one Nucleo-F746ZG and two NUCLEO-F767ZI boards, I have noticed that the captures strap values for Mode and Addr[0] often disaggree to the strapped values. The Phy LAN87xx requires the strap lines to be release...

STM32CubeMX - Power Consumption Calculator

Posted on September 02, 2016 at 13:38Hi,is there the possibility to change the ''Vdd Power Supply'' values inside of the Parameter Selection. I would like to select 2.8V but doesn't have the possibility to do so. Also small file hacks are welcome......

mr2399 by Associate
  • 3616 Views
  • 2 replies
  • 0 kudos

A confused problem about WWDG_IRQHandler

Posted on September 03, 2016 at 15:52 Hi, i'm studying stm32f407, but there is a problem puzzling methose days. It's about the WWDG. I just want to test the function of WWDG, so in my function which has been wrote to initialize the WWDG, i...

FLast.2 by Associate II
  • 1386 Views
  • 2 replies
  • 0 kudos

STM32F103TBU6 forgot port pins! restore comms?

Posted on September 03, 2016 at 15:34During my first foray into CubeMX I was distracted with clock settings and forgot to configure SWDIO/SWCLK and UART pins! After flashing, STLink can no longer connect. Is there a way to rescue the chip? 

MT9M001 Camera and DCMI

Posted on September 01, 2016 at 02:08  The original post was too long to process during our migration. Please click on the attachment to read the original post.

simfake by Associate II
  • 2001 Views
  • 3 replies
  • 0 kudos

RECIVE MESSAGE IN FIFO1 ON CAN BUS

Posted on August 30, 2016 at 16:45hi evry onei working on CAN protocol with stm32f103rbt6.it working so good.now problem is here: when i reading mailboxs of FIFO0 ،all think is ok but i can not receive the message from FIFO1.please tell me how to do...

l90mehdi by Associate II
  • 4034 Views
  • 11 replies
  • 0 kudos

stm32f427 flash dual bank in application programming

Posted on August 24, 2014 at 11:47Hi! I work with STM32F427 with 2 Mb flash size and want use high flash bank to load firmware image when upgrading.When I allocate firmware image in low bank (512kb) all works properly, but when i assign address to i...

abasovag by Associate II
  • 3300 Views
  • 9 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.