STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

PWM Frequency Change On the Fly

Posted on September 09, 2016 at 02:43I'm using an STM32F4 to generate PWM pulses. I need to do something a bit difference, the best way to describe it is like FSK ( frequency discontinuity not a problem if it occurs) For example - if one was lookin...

STM32CubeMX, cannot install FW package for STM32F4

Posted on August 09, 2016 at 08:58I am running CubeMX version 4.16.0, but I cannot update the firmware for STM32F4 to version 1.13.0.When I do: Help->Install New Libraries and tick 1.13.0 and then ''Install Now'', the installer runs until it looks l...

mats23 by Associate II
  • 2515 Views
  • 4 replies
  • 0 kudos

Trouble setting RTC from LSI to LSE on STM32F4

Posted on September 08, 2016 at 17:52Hi,I have a problem where I'm trying to detect the presence of the low speed external oscillator, and to use it if it is installed. On bootup, it does the following:   * Turn LSI on (it always defaults to off)   ...

gw by Associate II
  • 4106 Views
  • 7 replies
  • 0 kudos

STM7 - PWM in LP Mode(s)

Posted on September 08, 2016 at 13:15Hello All,Is it possible for the STM7x family to drive PWM outputs - specifically here TIM1 and TIM8 - in Low Power Mode?Thanks,John W. #stmf7-lp-pwm

stcom9174 by Associate II
  • 1325 Views
  • 3 replies
  • 0 kudos

STM7 - PWM in LP Mode(s)

Posted on September 08, 2016 at 13:16Hello All,Is it possible for the STM7x family to drive PWM outputs - specifically here TIM1 and TIM8 - in Low Power Mode?Thanks,John W.

stcom9174 by Associate II
  • 1044 Views
  • 3 replies
  • 0 kudos

FPU can not be enabled?

Posted on September 09, 2016 at 01:42Hi. I'm using the STM32F746G-Discovery board. I'm trying to make gcc output code that uses the FPU. The flags generated by my compiler settings when the FPU is supposed to be enabled are arm-none-eabi-g++ -mcpu=c...

RTC BQ32000 interfacing with stm32f030

Posted on September 08, 2016 at 12:47Hi I am trying to write some data to RTC register(say, day register) but unable to do so. If anyone knows,please provide some useful suggestions regarding what is the problem with the below code. // writing code ...

Usefulness of a bootloader

Posted on September 06, 2016 at 19:35Hi.I would really like to understand why bootloader is useful for? I read the document below, but still didn't get the point.http://www.st.com/content/ccc/resource/technical/document/application_note/b9/9b/16/3a/...

matic by Associate III
  • 4065 Views
  • 13 replies
  • 0 kudos

STM32MatTarget_V430: UsartRcv.slx

Posted on August 11, 2016 at 21:59 Hi there, I am using MATLAB/Simulink R2015b with STM32MatTarget V4.30 to access the USART. I generated also a software framework with STM32CubeMX 4.16 and the firmware package for the STM32F3 Family 1.6.0. It...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.