STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F746g-Disco slows down

Posted on September 24, 2016 at 14:58I have several stm32f746g disco mb1191b-02, and they are beautiful!I recently purchased stm32f746g disco mb1191b -04, but for my application slows down a hundred times. Keil compiler. How to make it work fast?

asfmail by Associate II
  • 3093 Views
  • 7 replies
  • 0 kudos

USART not getting enabled

Posted on September 24, 2016 at 17:57 Am trying to run USART by getting to write in the E-Terminal of CodeLite to interract with my STM32F4 However, i get no response when i the main method is called....here is my main method.... #i...

malehakim by Associate III
  • 1399 Views
  • 3 replies
  • 0 kudos

STM32F103 - rotary encoder TIM - INT generation

Posted on April 07, 2014 at 12:39 Hi. I successfully configured my STM32F103VC custom HW to use a rotary encoder by following the code suggested in this forum. So first of all: thank you! When I wrote ''successfully'' I mean that the cou...

nicola by Associate
  • 2585 Views
  • 5 replies
  • 0 kudos

Possible bug in HAL USART Driver

Posted on September 11, 2016 at 16:41I am experimenting with FreeRTOS and the HAL layer using an STM32F4 DISCO board.I have two threads.  One reads from the serial port and send the byte read, in a message to a second task.The second task, blocking ...

STM32L476 I2C speed setting accurately?

Posted on September 24, 2016 at 01:37Hi there,I got an issue recently when I was trying to set up the I2C speeds for STM32L476RG. I can set it up for an approximate value but never get the exact one. For example, I want to achieve 100 kHz while I ca...

jiayuan by Associate II
  • 3571 Views
  • 2 replies
  • 0 kudos

What SWD/ISP/JTAG to use with STM32F407?

Posted on September 24, 2016 at 00:16I am building a testboard with a 100pin 407VGT in it. There is no room for USB on it. After reading the HW manual I still don't know what is a correct/best programmer connector to use. There are 6 pins in Discove...

LMI2 by Lead
  • 3675 Views
  • 4 replies
  • 0 kudos

stm32L476RG nucleo dev board

Posted on September 23, 2016 at 20:00I am losing my mind, I start cubemx, installed stm32L4 library, configure the clock HSI , as this board has no HSE, GPIO and SPI, choosed MDK 5,  I generate the code, and try to test GPIO using Hal api, nothing h...

Declaring variables in External SRAM

Posted on September 23, 2016 at 18:33Hi everyone!  I'm having some difficulty getting variables to be declared in external SRAM.  I'm using a STM32L4.  If I do address casting like the FMC example project for the eval board in the library code I can...

Jim Kaz by Associate II
  • 2057 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.