STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Wrong entry point

Posted on September 27, 2016 at 12:47 Hello, I am using TrueStudio for STM My problem is, that when I start debugging the PC (program counter) shows an address of0xf3af48 As this address is somewhere in nomansland the Dissassembly shows ''...

machinist by Associate III
  • 1397 Views
  • 2 replies
  • 0 kudos

No interrupt from DMA

Posted on September 29, 2016 at 15:13 I'm trying to receive serial data using USART1 and DMA in 3 different chunks. Between I'm setting the buffer size in the DMA (2 bytes, 1 byte, 10 bytes) using the function set_ dma _buffer_...

heinz by Associate II
  • 1546 Views
  • 2 replies
  • 0 kudos

Prescaler Value for the Timer in Encoder mode

Posted on September 29, 2016 at 16:42I am using TIM4 of STM32F767 in Encoder mode. The period is set to 1000. The CNT value changes as follows: 0->1000->1->1000->0 and so on. On monitoring the DIR bit, I found that it keeps oscillating between 0 and...

Neo M by Associate II
  • 799 Views
  • 0 replies
  • 0 kudos

VCP driver issue for Windows 7. can recognize in Windows 10

Posted on September 16, 2016 at 23:29Hello all. Windows 10 can well recognize my STM32L1 device (custom PCB) as 'USB Serial device' but same isn't recognizing in Windows 7 (another PC). I've tried both VCP driver 1.3 and 1.4 in windows 7. Do I need ...

rumlyen by Associate II
  • 860 Views
  • 1 replies
  • 0 kudos

STM32F2 CAN Bus HAL Driver problem

Posted on September 29, 2016 at 12:29Hi This is my first post on this forum, so please excuse me if I don't follow the correct procedure. I think there are a problem with the STM32F2 HAL firmware driver version 1.4.0. I am using IAR Embedded workben...

pieter2 by Associate
  • 1545 Views
  • 2 replies
  • 0 kudos

Changing GPIO pin from IN <> OUT dynamically?

Posted on September 29, 2016 at 01:50What would be the best way to reconfigure a pin from Input to Output and vice versa on the flight?  The STM function HAL_GPIO_Init() is quite long so I would rather not use that function just to change a mode Inp...

Vu.Andy by Associate III
  • 9913 Views
  • 2 replies
  • 0 kudos

High Impedance Analog Input Specs

Posted on September 27, 2016 at 22:26I've been looking in vain all day for specs on the analog input GPIO. Any help or referral to the proper docs would be much appreciated.  It's referred to as 'high impedance', but 'high' is not quantified that I ...

Spike in AD conversions for STM32F407

Posted on September 20, 2016 at 10:35Hi, we have a problem in temperature AD acquisitions. The sensors are two Microchip MCP9700T-E/LT and are connected to ADC CH13 (pin &sharp18) end CH3 (pin &sharp26) through only a 22ohm resistance. The ADC is tr...

0690X00000603CEQAY.jpg 0690X00000602jcQAA.jpg 0690X000006035ZQAQ.jpg 0690X000006032eQAA.jpg

STM32F4 AD9833 SPI

Posted on November 02, 2014 at 11:38Hello,I'm using an STM32F4 discovery board and I'm trying to control the DDS waveform generator chip AD9833 with it. I'm not very experienced with ARM. I have a AD9833 module like in the picture:http://www.ebay.co...

shedili by Associate II
  • 4704 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.