Ask questions, find answers, and share insights on STM32 products and their technical features.
Posted on September 30, 2016 at 11:59Hi,I programmed simple GPIO high/low code on STM32F091VB through STVP but not getting any output from it. First, i configured BOOT OPTION BYTE then i was able to flash the microcontroller successfully. Refer att...
Posted on September 30, 2016 at 13:51Hello, Why are pins PB6 and PB9 connected to VDD through 4.7KOhm resistors in STM32F4-Discovery board?
Posted on September 29, 2016 at 23:10 Hi, I got two STM32 board which I'm trying to send data through one and receive it on the other board through bluetooth. I have configured the HC-05 as master and it connects to the HC-6 successfully....
Posted on September 30, 2016 at 12:50I am using a STM32L476 and I have a problem with de Vbus. It starts random to leak into de Vdd. I generate my code through CubeMXBackground: I am using a STM32L476JGY6. VDD-VDDA-VBAT-VDDIO2 running on 1V8VDDUSB ...
Posted on September 27, 2016 at 12:26Hi there,I build a Keil project for my STM32F103 MCU with STM32CubeMx.My goal is use the TIM1 channel 2 for control a Buzzer.I want to generate a PWM at 4KHz through TIM1 channel 2.I configured, with STM32CubeMx,...
95386
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.