STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Which interrupt for complete uart transfer with DMA

Posted on September 13, 2016 at 15:07Hi, With STM32L1, I need to know when a frame transmition is complete when sent on uart using DMA. By complete, I mean, the last bit has been sent on the line because I need to activate a buffer when data is tran...

JulienD by Senior
  • 1450 Views
  • 4 replies
  • 0 kudos

USB Hub controller interfacing

Posted on October 04, 2016 at 12:03Hey Guys, please anyone help to interface STM32F429VGT6 with the usb hub controller of TI. Anybody is having the program to communicate with the  USB hub controller? Is it possible to communicate with the many USB ...

dixon by Associate II
  • 560 Views
  • 0 replies
  • 0 kudos

Select STM32 for 3-Phase PFC?

Posted on October 02, 2016 at 23:06Hello,I design 3 phase PFC controller in very high power rate up to 800kW with another manufacturer microcontrollers. But nowadays I want to jump ARM area. In this case, I choose STM32F334 micro and working its dis...

STM32F429 GCC stack size error with personal DFU

Posted on October 03, 2016 at 13:52Hi everyone!I'm GUI programing with STM32F429GI.I've two application which one is myself DFU app and other is Main Application.DFU is located flash at 0x8000000 to 0x800BFFFAnd Main application start 0X800C000.STM3...

echonoh by Associate
  • 1404 Views
  • 2 replies
  • 0 kudos

Extract code from STM32F4DISCOVERY

Posted on October 03, 2016 at 08:33Hi, Can some one help me how to extract my code from STM32F4DISCOVERY KIT? I lost my code in my PC. I'm using IAR Embedded Workbench platform to program my STM32F4DISCOVERY KIT.

Resolved! STM32L073: RTC Wakeup event not exiting STANDBY mode

Posted on September 22, 2016 at 20:33I have the development board for the STM32L073 and have been testing the functionality of the board regarding waking up from STANDBY mode. I have been able to get it to wakeup only use the IWTG funcitonality. I h...

conner by Associate II
  • 3287 Views
  • 4 replies
  • 0 kudos

stm32f adc1 temperature

Posted on July 20, 2012 at 21:58I keep getting 0 void ADC1_Config(void){  ADC_InitTypeDef       ADC_InitStructure;  ADC_CommonInitTypeDef ADC_CommonInitStructure;  DMA_InitTypeDef       DMA_InitStructure;  /* Enable ADC1, DMA2 and GPIO clocks ******...

Multiflashing a stm32f030

Posted on October 03, 2016 at 11:21Hello,I'm using a st-link v2 to flash my stm32f030k6t6 chipI need to know if there is a way to multiflash download with the st-link utility tool?If not is there any way to do it, and how?Thank you #flashing-stm3...

ILI9341

Posted on October 01, 2016 at 16:51Hellohttps://twitter.com/tilz0R wrote this wonderful Lib for the Keil Toolchain http://stm32f4-discovery.net/2014/06/library-18-ili9341-ltdc-stm32f429-discovery/ Does someone know how to migrate this to Eclipse SW4...

ats3788 by Associate II
  • 1452 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.