STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

jpeg compression implement on stm32f4

Posted on October 20, 2016 at 12:49Hi everybody,I'm learning to do about the jpeg compression implement on microcontroller stm32f4. Could you help me if you did or know about this topic, please? Thank you very much for your enthusiasm!Best regards!

STM32F4 Problem with Timer OVF

Posted on October 19, 2016 at 07:28 Hi all, i have a problem with my program but i can not find the error. Maybe here is one who knows what i'm doing wrong. I want to meassure the time between two edges. I works most of the time, but some...

luk by Associate II
  • 1638 Views
  • 2 replies
  • 0 kudos

STM32H

Posted on October 20, 2016 at 13:55The website has some preliminary data for the 400 MHz STM32H74 now.

Reference manual in machine readable format

Posted on October 19, 2016 at 11:22I was wondering if it is possible to find the data in the programming and references manuals in machine readable format. The basics would be the peripherals, their registers, and their fields, but the list of IRQns...

unicycle by Associate III
  • 1077 Views
  • 2 replies
  • 0 kudos

Mistake in stm32f30x_gpio.h - V1.2.3

Posted on October 20, 2016 at 12:57Hello, there�s a mistake in the line 270 &sharpdefine GPIO_AF_2            ((uint8_t)0x02) /* COMP1_OUT, TIM1, TIM2, TIM3, TIM4, TIM8, TIM15, TIM16 */ The GPIO_AF_2 is NOT working for the TIM2, at least in the st...

airanzo by Associate II
  • 1285 Views
  • 1 replies
  • 0 kudos

STM32L476 SAI frame synchronization is incorrect swapped left right if HAL_SAI_Transmit_DMA is called 4 us after rising edge of WS

Posted on October 20, 2016 at 11:45 Hi All, I have an STM32L476RE connected to an audio codec. The audio codec is the master.SAI1_Block_Ais configured asSAI_MODESLAVE_TX,SAI_ASYNCHRONOUS,SAI_I2S_STANDARD,SAI_PROTOCOL_DATASIZE_16BIT,SAI_ST...

Ethernet receive failed

Posted on August 17, 2016 at 12:22Hi,I'm working on nucleo-f767zi with ethernet communication (LwIP stack).At startup (power-up or reset), randomly, the Ethernet module does not receive any frame.In other startup, it works fine.When it doesn't work,...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.