STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F20xxx Datasheet PA4/PA5 TTa or FT?

Posted on October 18, 2016 at 02:36Hi everyone, I'm a bit puzzled when I'm looking at the pinout part of the STM32F20xxx datasheet (p. 47). In there, it says that pins PA4 and PA5 are of type TTa (3.3V tolerant) BUT have a little note (4) saying ''F...

UART is not working properly at lower frequency

Posted on October 25, 2016 at 04:45Hi,I am using STM32F4xx MCU in our product and there is a GSM module connected over UART2 of MCU.Initially MCU was configured to operate at 168MHz frequency and UART2 was configured for 38400 baud rate. At that tim...

dj_v14 by Associate II
  • 3199 Views
  • 7 replies
  • 0 kudos

STM32F042F6- TSSOP20- Where is the TIMER 2 Channel 1?

Posted on November 01, 2016 at 17:28Dear all experts,I am programming Incremental Encoder Reading project for 2 encoders.I intend to use TIM2, and TIM3 for Encoder Config with 4X Reading. I check the datasheet (DM00105814) for MCU Pin configuration....

ADC+DMA+TIM: Sampling time

Posted on November 01, 2016 at 16:12Hi everyone, I have a general question regarding the sampling time when triggering ADC in DMA mode by using a timer event update. Let�s say I have a DMA buffer with size N. Is it possible to take one ADC sample pe...

reza by Associate
  • 1215 Views
  • 1 replies
  • 0 kudos

PWM input using InputCapture - Stm32Cube

Posted on October 29, 2016 at 11:30Hi everybodyI need to get PWM input value using input capture .I set Input Capture in Both Edge mode and I'm getting the HAL_TIM_IC_CaptureCallback very well . but for calculating the PWM duty cycle I need to know ...

software error keeps mcu in reset

Posted on November 01, 2016 at 15:11Recently I have observed an odd phenomenon: I have a code (which I believe is faulty) , I program the MCU (which initially is fully erased ) with that code; after that the MCU can not be reprogrammed by programmin...

ionutF by Associate III
  • 887 Views
  • 1 replies
  • 0 kudos

Code in stm32f427 or in stm32f429 ?

Posted on November 01, 2016 at 03:13Can I ask a question about programming stm32f427?I found the 427 and 429 are in the same manual. So, ignoring pin define, can I put stm32f429 code directly into stm32f427?Or I need to modify somthing in code? #...

ctc.ctc by Associate II
  • 1614 Views
  • 3 replies
  • 0 kudos

PWM WİTH DMA

Posted on October 20, 2016 at 07:50 Hi guys.I want to try pwm with dma.(by using burst)I tried to send data to timx_arr(period) that necessary for pwm. Still, ı observed from logic analyzer. But it has not signal without writing ''tim_timebasein...

NEO-6M STM32F103 Nucleo

Posted on October 29, 2016 at 17:55 Hi! I'm trying to communicate with NEO-6M GPS module by nucleo F NEO_6M starts transmitting date by itselfs, I've check TX signal on a scope and I can see frames. And now straight to the p...

bartocham by Associate II
  • 2840 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.