STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CubeMX Feature Request

Posted on November 29, 2016 at 22:26Hello, I like CubeMX and would like to suggest a feature for the report generator. I use Nucleo boards a lot for development and small projects and the support for it is really great, but I always have to look up ...

valtin by Associate II
  • 1158 Views
  • 1 replies
  • 0 kudos

STM32F303 SPI clock in read processing

Posted on November 10, 2016 at 06:14I have question about SPI communication on the STM32F303. Read processing from slave device(SD) in SPI does not go well. I expected that 1 is returned, but 0 is returned. I check program code and signal by oscillo...

kenji by Associate
  • 1472 Views
  • 2 replies
  • 0 kudos

Stm32f1xx and can problem + bug on CUBEMX library

Posted on November 24, 2016 at 12:52Hi, i have a little problem on Can program.If you call HAL_CAN_Init and after HAL_CAN_Deinit, when you call again HAL_CAN_Init, the function ''HAL_CAN_Init'' return always Timeout on CAN1.Its a bug ?And i found th...

Marco1 by Associate II
  • 944 Views
  • 2 replies
  • 0 kudos

STM32F769 Discovery emWin Hello World

Posted on November 24, 2016 at 21:42Hi,I’m  trying to use the STM32F769I_EVAL STemWin_HelloWorld project on the STM32F769 Discovery. Cube: STM32Cube_FW_F7_V1.5.0\Projects\STM32F769I_EVAL\Applications\STemWin\STemWin_HelloWorldThe application runs on...

paul2 by Senior
  • 696 Views
  • 1 replies
  • 0 kudos

STM32F7 Discovery: Encoder Interface & Getting access to PA9

Posted on November 22, 2016 at 21:42Hello, I'm trying to get the encoder interface operational on the STM32F7 Discovery Board. Unfortunately, there seems to be a lack-of-pins problem. It seems like the easiest timer to use is TIM1. Channel 1 is on t...

jasonj by Associate
  • 959 Views
  • 2 replies
  • 0 kudos

STM32F0 CAN Bus Busy Error

Posted on November 23, 2016 at 17:15 I'm working with CAN bus and sometimes my code stop receiving CAN Messages, only send. The function below /* Receive */ if (HAL_CAN_Receive_IT(CanHandle2, CAN_FIFO0) != HAL_OK) { /* Reception E...

eng23 by Senior
  • 1039 Views
  • 1 replies
  • 0 kudos

HSE clock bypass means?

Posted on November 28, 2016 at 03:20Recently, I read reference manual about stm32f4 rcc,but I have no idea about what is HSE clock bypass, I only know that there is a bit in RCC->CR for HSE BYPASS.I study the driver function RCC_HSEConfig()there are...

ctc.ctc by Associate II
  • 11590 Views
  • 5 replies
  • 0 kudos

LSE OSC Fail in STM32F107

Posted on November 27, 2016 at 07:22Dear,I am using STM32F107 with External 32KHz crystal and backup battery in my product.sometimes in power on, after:  RCC_LSEConfig(RCC_LSE_ON);then wait for LSE readey :while (RCC_GetFlagStatus(RCC_FLAG_LSERDY) =...

IDE and compiler for STM32L

Posted on November 08, 2016 at 09:37Hi,I've installed Coocox CoIde and ARM GCC compiler. But I cannot create new project in Coocox IDE as it shows error message in repository. I've STM32L152 discovery board and I've tried example codes provided. It ...

ashelke by Associate
  • 1134 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.