STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

DFSDM conversion resolution problem

Posted on December 08, 2016 at 22:32Hi,I am trying to build something and currently doing some evaluation and development with 32L476GDISCOVERY Discovery Kit with STM32L476VG microcontroller.What I am trying to achieve at the moment is output of int...

stm32f3/4 maximum gpio read write operation

Posted on November 09, 2016 at 18:55HelloAs i inspected through assembly instructions, it is possible to read 16 bits gpio port with 2 cpu cycles and write with 4 cpu cycles, beside of electrical considerations, is it possible to achieve reading and...

DMA on SPI

Posted on November 11, 2016 at 14:20Hello,I have one question. I have two CPUs (STM32F407 + STM32F103) and I need to ''share'' (or better say ''synchronize'') 64 bytes between these CPUs every 100us. So every 100us the CPU must send 64 bytes to anot...

Bad SPI clock duration in stm32f746

Posted on November 11, 2016 at 18:08Hello. I have got stm32f746 and I make project with cubeMX. I  want to use SPI4, SPI5, SPI6 as fullduplex master with 50Mb/s baudrate. Then I try to HAL_SPI_Transmit(&hspi4, pData, 1, 30000); in while(1) cycle. ...

ldpr by Associate
  • 1713 Views
  • 2 replies
  • 0 kudos

STM32F3 - Sending Sine Wave with DAC and DMA

Posted on November 29, 2016 at 05:51 Hello! I am currently trying to send a sine wave through the DAC. I've tried both using the std peripheral libraries and stm32cube, but to no avail. The frequencies and amplitude of the measured sine w...

kl4971tse by Associate II
  • 3633 Views
  • 4 replies
  • 0 kudos

How do I switch PLLSource once it is running?

Posted on December 07, 2016 at 22:19Hi, I want to start off my STM32F745VET6 running on the PLL sourced from the 16MHZ HSI oscillator. I need to run some I2C code to initialize an external multi-output high accuracy clock generator chip where one of...

STM32F042F6 SPI1 clock polarity problem

Posted on November 14, 2016 at 08:53Hello,On my currently developing device and I issued a problem. I'm using CubeMX 4.17, F0 package 1.6 and F4 package 1.13.1.I developed the code for F4 - SPI1 communicating with NRF24L01+ module using HAL library ...

help srf04 stm32f407

Posted on December 10, 2016 at 11:23hi allwhile (1) { int time; int i=0; GPIO_SetBits(GPIOA,GPIO_Pin_1); //delay_us(10); Delay(240); //Delay01ms(100); GPIO_ResetBits(GPIOA,GPIO_Pin_1); while(GPIO_ReadInputDataBit(GPIOA,GPIO_Pin_0)==0); while(GPIO_Re...

kakaducsy by Associate II
  • 1262 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.