STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI CRC problem with dma on stm32f0

Posted on December 31, 2016 at 10:06HelloI have connected two uc through SPI .My target is to send data with DAM+CRC.one of them is slave stm32f030 and the other one  is stm32f429.I'm using cubeMX for confige spi and dma  registers .Here is slave co...

Resolved! STM32L152C6 Enter STOP Mode

Posted on December 28, 2016 at 10:22The original post was too long to process during our migration. Please click on the attachment to read the original post.

kaloyan by Associate III
  • 1673 Views
  • 2 replies
  • 0 kudos

Problem with ADC Timer Trigger.

Posted on January 02, 2017 at 10:11I am trying to get the rate of change of value of the potentiometer using ADC with a timer trigger. So far I have failed. I am trying to measure the change in value of ADC with the Timer trigger of every 100 micro ...

A few questions on goto-statements, encapsulation, etc

Posted on December 31, 2016 at 23:25I am working with the STM32F405 microcontroller and I am trying to have a software UART use the same interrupt line (EXTI15_10_IRQn) as other interrupts (for example, button press interrupts). In a perfect world, ...

arnold_w by Senior II
  • 2148 Views
  • 5 replies
  • 0 kudos

STM32F7 series need separate SDMMC PLL

Posted on December 31, 2016 at 19:56Hi all. The standard SDMMC bus speed is 24MHz which, on the STM32F7 series, is derived from the USB PLL48 clock source / 2. If we want to operate the SD card in High Speed mode, which has a maximum bus speed of 50...

STM32F4 corrupt memory/damaged MCU

Posted on August 30, 2015 at 16:53Hello,I've been working on a project on my STM32F4 Discovery for a few weeks now and it's been working fine. Today I connected a OV7670 camera and after uploading the code the discovery stopped working after a while...

azayetey by Associate II
  • 2021 Views
  • 3 replies
  • 0 kudos

Debugger doesn't halt at main()

Posted on December 30, 2016 at 06:03Hi,I am using STM32F4xx based custom board and IAR as an IDE for development. Till now everything works fine, but after adding few lines of code the debugger has stopped working i.e. it is not halting at main(). I...

dj_v14 by Associate II
  • 3158 Views
  • 5 replies
  • 0 kudos

Resolved! Understanding SPI on the STM32F3

Posted on December 29, 2016 at 19:44Hi, I have a NUCLEO-F303 board which I would like to use to communicate to two devices using SPI. The NUCLEO would be sending and receiving data to and from the devices via MOSI and MISO.Looking through the datash...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.