STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F72 and STM32F73 reference manual?

Posted on February 19, 2017 at 09:48I'm wondering where to find reference manual for STM32F72 and STM32F73 chips? I was able to find the datasheets - directly from the site of the particular chip - but the reference manual is not available from the ...

Define interrupt handler as weak

Posted on February 22, 2017 at 10:31I need to define my own interrupt handler. Cube not not generate the ISR as weak so everytime I regenerate the code with cube, I have to modify the code to hide the interrupt handler generated by cube.Would it be ...

Adalgiso by Associate II
  • 3023 Views
  • 4 replies
  • 0 kudos

trace error in stm32f411 Discovery Board in true studio

Posted on February 23, 2017 at 07:52Hi,I have configured stm32f411 I/O & clock & etc. in STM32CubeMXand generated source code in true studio.After that, I have connected stm32f411 discovery board and started debug in true studio.Then when I trace by...

Possible reasons for STM32F4 to generate a reset.

Posted on February 22, 2017 at 12:26We have a strange problem on one of our boards. One cabinet has 3 identical boards, running the same binary, (the application is configured remotely from the main server so the software behavior is different), but...

Maor Avni by Associate II
  • 1336 Views
  • 1 replies
  • 0 kudos

STM32F1 how to configure CAN filters in ID List mode?

Posted on February 21, 2017 at 10:06I can configure CAN filters from main.c file, but I want also to configure them by sending frame from the other node. It's that even possible to configure CAN filters while STM is working? There is the code from i...

jerzy by Associate II
  • 5489 Views
  • 5 replies
  • 0 kudos

Resolved! STM32 1MBaud UART

Posted on February 22, 2017 at 14:32Hello, I am currently using the STM32L432KCU6 and I am finding a bottleneck when streaming from the UART.  I need around 1MBaud but according to the datasheet the STM32L432KCU6 max is 200kBaud.  At what family of ...

An issue about stm32cubemx

Posted on February 15, 2017 at 00:36Recently, when I tried to create a new project or load an existing project using the latest version (4.19.0) of cubemx, it kept going back to the homepage. I can't figure out why. Does anyone know how to fix this ...

Configure Timer for Output Compare

Posted on February 22, 2017 at 15:10 I want to configure TIM3 on my STM32F072 to count the number of pulsesfrom the built-in comparator, and thenToggle Pin PA7 when the compare value was reached. I have a multiplexed sine signal coming into the c...

abotha by Associate III
  • 795 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.