STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F0xx findings

Posted on November 14, 2016 at 22:07In a new project there are several identical STM32F031 devices in a role of a slave mcu, driving LEDs and reading in various input signals. As their functionality is very similar, it is tempting to have only one s...

Interleaved ADC

Posted on February 23, 2017 at 00:04Device: STM32F437I am using ADC3 channels 5 (rank 1) and 8 (rank 2) in interleaved mode, the input for channel 5 is 0 volts and the input for channel 8 is near upper limit. Trapping after the first interrupt the 3...

John Hite by Associate III
  • 1456 Views
  • 2 replies
  • 0 kudos

STM32F746G-DISCO Error Device DS1307 not connected

Posted on February 24, 2017 at 11:45I have new STM32F746G-DISCO but when i powered the board , the LCD shown this error messageError DetailERROR: Device DS1307 Not Connected ProperlyAny ide what's wrong or how to get rid this error? Thanks#stm32f746...

STM32F103 - No Internal pull-up on the NRST pin

Posted on February 23, 2017 at 11:48Hi,In the current datasheet of STM32F103 (DocID13587 Rev 17) it is written:5.3.14 NRST pin characteristics The NRST pin input driver uses CMOS technology. It is connected to a permanent pull-up resistor, RPU (see ...

samuel23 by Associate III
  • 3636 Views
  • 6 replies
  • 0 kudos

Timer Input capture Filter

Posted on February 09, 2017 at 13:38Hey,I'm using the Input Capture of TIM8 to measure the period of a signal. The Timer runs at 16MHz and the MCU (STM32F405) at 144MHz. I'm also using the ICFilter at the moment. The value is set at 0x02. My questio...

luk by Associate II
  • 2403 Views
  • 3 replies
  • 0 kudos

Bare minimum register settings for SPI on STM32F103

Posted on February 23, 2017 at 19:53Hello,I have need to bring up SPI1 (PA4,PC5,PC6,PC7) on an STM32F103 in master mode using the least code possible. I have a function that (is supposed to) initialize the SPI. I am using the bit-band region to mani...

Resolved! HSI, HSE, LSI, LSE and clock nonsense

Posted on February 22, 2017 at 22:05Hi,I'm working on a stm32F101CBT6.The board has a 16 MHz HSE (connected to PD0.PD1) and a 32.768 KHz LSE (connected to PC14/PC15).The board will use SPI1, SPI2, USART1, USART2, I2C1 and a few GPIOs.I've worked wit...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.