STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! how can i solve it ?

Posted on February 27, 2017 at 06:38I have a problem.the problem is please install truestudio toolchain to open the project or associate the file type of the project with your toolchain in system default program settings.i don't know how can i solve...

DMA transfer count

Posted on February 27, 2017 at 07:07Since the Wish List seems to be closed, I'll put this request here.To the processor designers:The DMA transfer count is a 16 bit value that can be in the range 1-65535. Since 0 is a useless value and 65536 would b...

STM32F3 opamp in PGA mode: DC conditions

Posted on February 27, 2017 at 04:34GreetingsI'm trying to determine how I set the DC conditions (i.e. input bias) on the +ve input of an opamp on the STM32F3 series when all the feedback is internal during PGA mode. If I set the input to half way b...

STM32F4 Precision measure period of a signal

Posted on February 26, 2017 at 20:30Hello all,i need to measure an external clock source of 32768hz  with little variation as posible... this means to measure as true as possible,  with variations  maximum of +/- 2hz ...Is this achievable with  inpu...

Bogdan by Senior
  • 2461 Views
  • 5 replies
  • 0 kudos

Can't debug CUBEMX generated code

Posted on February 26, 2017 at 01:52Hey, I got Discovery F3 board, i wanted to start project which uses I2C communication, so i enabled I2C1 peripheral and generated code for EWARM IDE using CubeMX. I uploaded code on board and pressed GO in debug o...

Resolved! fresh Custom HID Project, not flashable on my STM32F4

Posted on January 21, 2017 at 13:33Hey guys,I created 2 sets of projects with CubeMX for my STM32F429I-Disc 1 board.I project is a Device HID project, the other one is a Device Custom HID project.The Device HID projects works fine, the Custom HID pr...

Resolved! STM32L432 - I2C Address Off By 1-Bit

Posted on February 24, 2017 at 06:55 Hi, I recently brought up the I2C using the STM32CubeMx(4.0) and STM32CUBE_FW_L4_v1.6.0 and I was attempting to write to a slave device with an address of 0x2A. I noticed that my slave device was NACK-in...

0690X00000606OSQAY.png 0690X00000606OXQAY.png 0690X0000060678QAA.png
Nolan L by Associate III
  • 6293 Views
  • 4 replies
  • 0 kudos

Resolved! STM32F303: GPIO configured with PP affect ADC readings

Posted on February 25, 2017 at 04:22Hi,I'm using a STM32F303 (landing page: http://www.st.com/en/microcontrollers/stm32f303k8.html) for one of my project. I have PA0 configured as a GPIO output with push pull used to turn ON/OFF a BJT. I also have P...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.