STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB mass storage with sd card

Posted on February 28, 2017 at 12:53hello all,i am working on stm32f4-discovery.i want to implement mass storage functionality using usb.i want to share sd cards data to PC using USB.i have implemented code for sd card in 1-bit.but now i want to imp...

stm32f7 discovery about play wave file 8khz

Posted on February 28, 2017 at 12:20Dear,i am using stm32f746 discovey board. I open Audio_playback_and_record application at STM32Cube_FW_F7_V1.6.0 with IAR complier and modify code with Audio Play for sample 8khzAfter  i copy wave file with 8khz s...

The Microcontroller programs but it's not working!

Posted on February 27, 2017 at 15:46Dear Friends,I have designed two identical PCB boards and I used stm32f103rbt6 microcontroller.One of them works properly but the other one has a problem which I cannot understand.The micro programs successfully b...

Mujtaba by Senior
  • 2323 Views
  • 7 replies
  • 0 kudos

Any ideas with regard to spurious ADC values

Posted on February 27, 2017 at 20:05I am using the ADC+DMA to collect samples for AC power calculations.  The voltage and current are well buffered (low impedance sources) sampled at about 7kHz.The data acquisition will work properly for many second...

Single ADC/DMA multi-channel setup

Posted on February 28, 2017 at 00:06Device: STM32F437The code I am working on was setup to use interleaving but after doing some reading I get the impression that interleaving is only for multiple ADCs and we are using 2 channels on ADC3. So it seem...

John Hite by Associate III
  • 1254 Views
  • 2 replies
  • 0 kudos

STM32F302RE Hard fault handler

Posted on February 27, 2017 at 10:07Hi all, I am using a STM32F302RE MCU with a customised board. My code works find when I run it at normal temperature. However, when I test it at 55 degrees, the code goes to Hard fault handler after the line in th...

akshayamk by Associate II
  • 1551 Views
  • 3 replies
  • 0 kudos

Resolved! STM Flash Loader Demo Tool not Working.

Posted on February 27, 2017 at 23:45I want to flash a load on the STM32F0CB using the STM Flash Loader demo. My configuration is: 57600, Data Bits:8, Parity: Even, Echo: Disabled, Timeout: 10.I also tried with parities Odd and None.After resetting t...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.