STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Power and STM32s

Posted on March 13, 2017 at 09:08HelloOur team is using STM32F103R8T6 and STM32F405R8T6 for a robot and for some reason sometimes when we turn the power on (from battery or a DC power Supply) the MCUs short from the inside and when we change the hea...

0690X00000606XZQAY.png

STM32F4 PLL I2S continous clock generation

Posted on March 12, 2017 at 00:13Hello,i have a question about MCLK and LRCK generation on an STM32F4 system.I want to connect an Audio ADC to an SPDIF codec which need an continousMclk and Lrclock. I have the option to use an external 24.5760 Meg c...

Stop mode, wake up questions

Posted on February 08, 2017 at 11:29Hi ! I am using an STM32l0xx and I have some questions about stop mode. First can I choose by software  which exti line are going to wake up the STM. Then can I have a timer interrupt each minute for example but o...

STMCUFinder does not list JPEG codec

Posted on March 15, 2017 at 11:53Hello,as of today, the STMCUFinder does not list the JPEG device as a selection criteria  on the left. So if anyone is iinterested to find a device with that CODEC, more digging is needed.Regards

STM32F407's Clock is not working

Posted on March 14, 2017 at 12:31dear. Engineer sirWe are currently working on a project using the STM32F407ie UFBGA176 chip.After configuring the microcontroller on the PCB and checking the operation of the microcontroller, the external oscillator ...

0690X00000602RSQAY.bmp
rui CHU by Associate II
  • 2581 Views
  • 5 replies
  • 0 kudos

USB bootloader serial number

Posted on February 20, 2017 at 12:37Hello,can the information be made available how the on-chip USB bootloader generates the serial number?This would be helpfull when an application provides a DFU endpoint to jump to the built-in USB bootloader.  As...

Is it possible to use Encoder and PWM from the same timer?

Posted on March 13, 2017 at 18:05Hi all,I am new to the STM32 and I am struggling with determining whether or not I can get PWM and Encoder input working on the same timer.I have a Nucleo-F103 board and using CubeMX, I have set up my board to use Ti...

Aaron M by Associate
  • 3092 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.